Connecting with a Wireless World
By Greg Quirk
A mesh network is a way to ensure that data is
properly conveyed to other systems within the
network. This is an expansion on point-to-point networking because if a device in the chain is broken or fails,
it does not disrupt the data transfer. Each device creates a “node” that can create unique information but also
passes data from other devices within the network along. Previously, mesh networks were hardwired, but
wireless networks are sufficiently low in power and cost and robust enough to ensure a solid
connection.
Revenue and Shipments
The use of mesh networks has grown substantially since they were first introduced. The current estimations expect
revenues to exceed $7 billion by 2014 with a 100 percent growth in municipal infrastructure in 2010 alone. When
you take into account that there were over 8 million smart meter shipments in North America in 2009, this is
quite a significant growth rate. Nearly 70 percent of the average utility bill could be influenced by wireless sensor networks , according to reports, and could control
heating and lighting to reduce energy costs.
Applications
There are many applications for
mesh networks aside from the military, which is where the technology first was implemented. Industrial systems
rely heavily on the assurance that the critical information they use to operate efficiently is always available.
For example, smart gas meters use mesh networks to ensure that billing information is sent even if there is an
issue with some of the meters between the home and the receiver.
Asset tracking is another application where it is vital not only to know where shipments are within the chain of
custody, but also to guarantee that nothing gets lost in the process. This is another huge growth area that is
projected to reach $845 million by 2014, which in turn can save companies millions through its implementation.
Implementations
Two of the most common kinds of wireless networks are ZigBee and Wi-Fi,
but there are many others that have earned their right in this space. There was a controversial study performed
by GE that demonstrated that ZigBee systems consume just 0.39 watts over 24 hours, compared to 0.87 watts used
by Wi-Fi solutions. While the amount may seem small given the size of the networks, this can equate to over $315
million when implemented in one billion devices. There has been some debate over the validity of the report, but
it is clear that this is a hot topic for many people.
ZigBee
ZigBee was created with a mesh topology in
mind. It leverages extremely low power consumption to ensure that the network operates for a very long time on a
single battery, typically years before needing to be changed. It can operate in the ISM band, as well as the
2.4GHz range.
The Laird
Z100S1 , with an external antenna, has an outdoor range of 4.8km.
There have been some changes to the ZigBee stack. To make setting up the network easier, companies such as DIGI
have created a programmable module that makes creating
ZigBee applications easier by including a processor separate from the RF code.
SNAP
SNAP is an abbreviation for
Synapse Network Application Protocol. SNAP
has a very small memory footprint of only 40 KB, so more memory is available for other applications.
The Panasonic PAN4561 , an
application compatible solution with
Panasonic PAN4455, offers extended range by using low noise and power amplifiers. CEL produces a single-chip RF transceiver with RF transceiver
with baseband modem, a hardwired MAC and an embedded 8051 microcontroller with internal Flash memory for a
complete solution.
WirelessHART
While there are 30 million HART devices in place, until the inclusion of WirelessHART, they were not used to
their full potential or set up to provide device diagnostics. The wireless aspect enables the devices to be
placed in more locations than before, while obtaining the full benefits that HART offers.
A transceiver module for WirelessHART is offered from RFM. The XDM3620HP , which
requires no embedded
programming, is designed for industrial applications where long battery life is required.
Alternatives
Other solutions in the mesh networking arena include BlueTooth, Ultra Wide Band, wireless USB, and IR. So far,
there is no single solution that meets all of the market’s needs, although new developments are being made in
all products to provide better coverage at a lower price while consuming less power. And while it will be years
yet before there is a “winner” in this space, the industry is still moving forward to take advantage of the many
benefits that mesh networking offers.
Greg Quirk has been a technical writer since 2004 focusing on semiconductor
components, consumer devices and business trends. He has written numerous articles for industry
publications and presented at technical conferences. His expertise has been sought by the financial
community on multiple occasions to predict design-wins in popular consumer products.