Solving Data-centric Challenges with Intel® Agilex™ FPGAs
Image Source:
Intel®
By Adam Kimmel for Mouser Electronics
Published November 9, 2020
With the constant expansion of the Internet of Things (IoT) and ongoing rollout of 5G broadband networks, evolving
IT strategies and roadmaps continue to include edge computing. This emphasis led Gartner to project in its
article, What Edge Computing Means for Infrastructure and Operations Leaders, that enterprise edge
computing will grow from 10
percent to 75 percent by 2025 through micro-data centers and cellular networks. Data-centric
applications, such as 5G and edge computing need to process larger amounts of data, creating the need for
advanced processing technology.
Data needs to travel across the entire IT infrastructure, from application to network core to data center and
back. Because each end-user application is different, system architects need customizable, flexible data
processing to optimize cost and energy efficiency at the point of data generation. Intel®Agilex™ FPGAs combine FPGA flexibility with
application-specific integrated circuit (ASIC)’s efficiency and performance levels. This new solution
integrates a wide range of semiconductor elements into one system.
Intel® Agilex™ FPGAs
Built on Intel’s 10nm SuperFin Technology, Intel® Agilex™ FPGAs provide flexibility
and agility beyond previous generation FPGA devices, making them ideal for Industry 4.0 (Figure
1).
Figure 1: Intel® Agilex™ FPGA offers
flexibility and agility to support edge devices, low-latency, and high-bandwidth. (Source:
Intel®)
Three product variants exist within the Intel® Agilex™ portfolio: Flexible (F-series), Interface
centric (I-series), and Memory centric (M-series). Intel® Agilex™ F-Series FPGAs feature transceiver
rates up to 58Gbps, PCIe Gen4 x16, 400Gb Ethernet hard IP, and DDR4 External Memory Support using hard memory
controllers. Intel® Agilex™ I-Series FPGAs increase the maximum transceiver rate to 116Gbps, and also
include PCIe Gen5 x16 and Compute Express Link (CXL) hard IP. Intel® Agilex™ M-Series FPGAs
add support for in-package HBM2 memory, DDR5 External Memory Support, and Intel® Optane
Persistent Memory support.
Architecture and Design Philosophy
The innovation in the Intel® Agilex™ FPGA is in the integration of flexibility and agility.
Engineers combined a general-purpose, high-performance FPGA core fabric with function-specific chiplets in a
single package to create a flexible device architecture. The traditional FPGA fabric makes the product flexible
enough to extend to multiple applications. This integration makes the Intel® Agilex™
flexible to support a wide array of applications.
Although earlier commercial FPGAs contained a single monolithic die or multiple instances of the singular die,
Intel® Agilex™ leverages advanced packaging technology to enable various unique silicon
dies within the package.
This enables Intel® Agilex™ FPGAs to excel in four important areas: design re-use, transceivers,
interfaces, and compute/AI. Intel® Agilex™ FPGAs utilize the second generation Hyperflex core
architecture, allowing design and IP reuse from previous generation Intel® Stratix® 10 FPGAs while
offering up to 40 percent higher performance or up to 40 percent lower power dissipation. Both products use the
same Quad-core Arm Cortex A53 hard processor preserving investments made in both software and peripheral
design. Intel® Agilex™ FPGAs offer transceiver rates up to 116Gbps PAM4 and 58Gbps NRZ, supported by
PCIe, CXL and 400Gb Ethernet hard IP to allow efficient implementation of a wide variety of serial protocols and
interfaces to optical modules, processors, and other devices. For compute-intensive DSP applications, Intel®
Agilex™ FPGAs feature a Variable Precision DSP block with hard fixed-point and hard floating-point modes
of operation, including FP32, FP16, INT18/19, INT9 and BFLOAT16 number formats that support a variety of
applications including AI training and inference.
New Capabilities Unlock New Applications
The features described above illustrate the benefits and capabilities of Intel® Agilex™ FPGAs. Their
flexible yet agile design makes Intel® Agilex™ FPGAs ideal for acceleration applications in the data
center with both PCIe and CXL processor attachment, new DSP functions for AI, high-performance external memory
interfaces such as DDR4, DDR5, and Intel® Optane™ persistent memory, and in-package HBM2 memory. Other
applications for Intel® Agilex™ FPGAs include cloud infrastructure, network function virtualization
(NFV), automotive, aerospace, manufacturing, and military.
Conclusion
Intel® Agilex™ FPGAs offer a disruptive approach to FPGA architecture, integrating logical design
flexibility with customizable agility. Intel® Agilex™ FPGAs deliver on the promise of the Intel
acquisition of Altera with impressive advancements in silicon and solutions, enabling a broader market while
staying true to the well-established FPGA user community. This transformative device’s efficiency and
performance gains will dramatically improve the user experience and can elevate your brand and product portfolio
to a position of strength in new and emerging markets.
Author Bio
Adam Kimmel has
nearly 20 years as a practicing engineer, R&D manager, and engineering content writer. He creates white papers,
website copy, case studies, and blog posts in vertical markets including automotive, industrial/manufacturing,
technology, and electronics. Adam has degrees in Chemical and Mechanical Engineering and is the founder and
Principal at ASK Consulting Solutions, LLC, an engineering and technology content writing firm.