Elektronik Bileşenler
Zorlu koşullara karşı hazırlıklı olun
Endüstriyel Otomasyon
Endüstriyel Otomasyon parmaklarınızın ucunda
RF Power amplifiers are necessary to maintain reliable, long-range communications. (Source: Qorvo)
5G is one of the most important and powerful technologies ever to reach the market in the field of wireless communications. Offering significant improvements in data rates, latency, and capacity as compared to 4G, 5G is poised to be a truly transformative technology in the industry and the world.
Yet, these radical performance improvements generate an increased strain on and tighter requirements for the underlying radio-frequency (RF) hardware. One of the most instrumental pieces of RF hardware is the power amplifier (PA), a device whose importance has only increased with the proliferation of 5G. To help ease the challenges of designing RF PAs for 5G, power amplifier modules (PAMs) have become an important tool in recent years.
In this post, we’ll talk about PAs, their role in 5G, and how Qorvo leverages PAMs to help support the 5G infrastructure of the future.
When working with RF signals, especially at the higher frequency bands of 5G, voltage levels can be extremely low. This is a challenge because the electromagnetic (EM) signal becomes more susceptible at lower amplitudes to the effects of system-level noise (i.e., signal-to-noise ratio decreases). On top of this, lower-voltage signals generally lack the strength necessary to drive downstream circuitry or antennas.
To address these challenges, engineers use PAs. An RF PA is a circuit block that serves to increase the amplitude, power output, or drive capacity of an RF signal. Generally, RF PAs live near the system antennas to provide a transmitting antenna with a high-power signal.
With a PA, the goal is to boost the signal while maintaining a high level of fidelity from input to output. For these reasons, linearity, efficiency, and output power are important specifications for a PA.
Historically, PAs and their surrounding circuitry were designed using discrete components on a board. While this approach has served the industry for many years, the efficacy of this approach is coming into question as several nontrivial design challenges emerge.
One of these challenges is being able to balance the tradeoffs among area, cost, performance, and power consumption. Generally, these specifications tend to conflict with one another, and designers must know how to optimize their circuits to balance the tradeoffs in an optimal way for their given application. Balancing these tradeoffs is increasingly difficult when using discrete components as considerations like part selection, component interoperability, and layout impact performance.
This is further confounded when moving to 5G, where systems need to cover wider bandwidths and higher frequency ranges. Today’s systems require an average instantaneous bandwidth of up to 400MHz while operating at frequencies up to 4GHz. The challenge is now maintaining the aforementioned system tradeoffs while also providing performance over this frequency band.
To address these challenges, Qorvo has turned to PAMs.
A PAM is an electronic component that integrates the discrete components in a PA, and its surrounding circuitry, into a single packaged solution. For example, in the application of a 5G base station, a PAM might integrate the driver amplifier and final stage amplifier into a single package as opposed to implementing them as discrete circuit blocks. By integrating the entire PA system onto a single module, we can achieve many important results (Figure 1).
Figure 1:The Qorvo QPA4501 PAM incorporates a Doherty final stage for high power and efficiency. (Source; Qorvo)
First, PAMs make the design of RF systems, such as base stations, significantly easier than the discrete option. Instead of selecting components and designing a discrete circuit, designers can instead select a module that fits their needs and implement it within their system as a whole.
Beyond this, PAMs can offer improved performance and area when compared to non-module solutions. By integrating the components, layout concerns, such as parasitics, can be minimized, resulting in higher performance and efficiency. Qorvo PAMs also address considerations like impedance matching for the designer, ensuring that maximum performance is attainable.
Lastly, this integration allows for smaller systems on average, saving weight and area for users in their final system design.
Qorvo offers the industry’s largest, most innovative GaN-on-SiC portfolio to help users realize superior efficiency and operational bandwidth. The GaN-on-SiC products deliver high power density, reduced size, excellent gain, high reliability, and process maturity. Qorvo recognizes the importance of PAMs in the future of 5G system designs and is working to bring industry-leading solutions to the market. Qorvo’s PAMs aim to offer a balance of power, efficiency, size, and cost while making the design as easy as possible for the users.
Shawn Gibb is a Sr. Product Line manager for 5G base station products within the Infrastructure and Defense Products business unit (IDP) at Qorvo. He has extensive experience in both product development, and materials and device technology development. Shawn has a B.E. in Chemical Engineering and M.E. in Materials Engineering from Stevens Institute of Technology and holds 29 patents in III-Nitride materials and device technology. Prior to joining Qorvo in 2019, Shawn worked at Akoustis, Crystal IS, RFMD, and Emcore corporation.
Qorvo supplies innovative semiconductor solutions that make a better world possible. We combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve our customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including consumer electronics, smart home/IoT, automotive, EVs, battery-powered appliances, network infrastructure, healthcare and aerospace/defense. Visit www.qorvo.com to learn how our diverse and innovative team is helping connect, protect and power our planet.