Mouser Electronics - Elektronik Bileşen Distribütörü
 
Türkiye - İşaretle Türkiye

Lütfen para birimi seçiminizi onaylayın:

Euro
Incoterms:FCA (Nakliye Noktası)
Gümrük vergisi, gümrük ücretleri ve vergiler teslimat sırasında tahsil edilir.

ABD Doları
Incoterms:FCA (Nakliye Noktası)
Gümrük vergisi, gümrük ücretleri ve vergiler teslimat sırasında tahsil edilir.

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Quantum Computing Paves a Smarter Path to Resource Optimization Liam Critchley

(Source: Bartek Wróblewski/stock.adobe.com)

Quantum computing holds great promise for revolutionizing the way industries manage and conserve resources. From energy grids to data centers, quantum systems promise to deliver faster, more efficient solutions that could significantly reduce energy consumption and environmental impact. But as with any new technology, the road to widespread adoption comes with unique challenges.

In this blog, we dive into how quantum computing can transform resource optimization across sectors, with a special focus on energy efficiency, sustainability, and the challenges that lie ahead.

The Quantum Advantage in Resource Optimization

At the heart of quantum computing lies its distinctive capability to solve multiple problems simultaneously through the superposition of qubit states. With this ability, quantum computers can outperform classical systems in speed and efficiency, especially when tackling optimization problems.

Perhaps the most transformative impact is expected to be in the energy sector, where quantum computing can optimize everything from grid operations to developing more sustainable energy production. Even energy-intensive processes like machine learning (ML) could become more sustainable, thanks to quantum computing’s ability to perform calculations faster and with less power. So, regardless of whether it’s optimizing the energy industry itself, or helping to conserve energy resources in other industries, quantum computers could help to improve resource use and advance sustainability efforts on many fronts.

Improving Energy Grid Efficiency

As energy infrastructure works toward more advanced smart grids, solutions are being sought that optimize diverse grid operations, from balancing supply and demand and developing advanced renewable energy forecasting to predicting grid needs and improving energy storage. By performing faster calculations and accounting for a multitude of factors, as well as its ability to solve multiple problems simultaneously, quantum computing offers such solutions. With the increasing integration of decentralized smart grids, quantum computing can address many different grid challenges—such as load balancing and fault detection—due to predictive modeling and analysis capabilities that show significant improvements over classical systems.

Enhancing Demand Response and Battery Longevity

In periods of high demand or low energy generation, energy storage systems play a critical role in maintaining grid stability. Quantum computing can optimize when and how these systems are used, ensuring energy is deployed only when necessary.

This not only improves grid resilience but also extends the lifespan of batteries by optimizing their charge and discharge cycles. Fewer replacements mean less waste and lower resource consumption over time.

Forecasting Renewable Energy with Precision

Another key area where quantum computing can assist with improving energy grid efficiency is through better prediction of renewable energy forecasts. Renewable energy sources like wind and solar are inherently variable. Quantum computing can take data from weather models—such as wind speeds and solar irradiation—historical trends, and environmental sensors at much larger scales than classical computers in order to build more robust forecasting models. With better forecasting models, grid operators can better anticipate renewable energy demand to adapt grid operations and ready battery energy storage systems (BESS) for storing energy during increased supply periods, ensuring there are enough resources in low harvesting periods. Additionally, quantum computers can maximize which renewables should be used at different times based on demand, stored energy levels, and anticipated maintenance schedules.

Real-Time Grid Optimization

Beyond forecasting, quantum computing can optimize grid operations in real time. It can identify energy bottlenecks, detect faults, and balance supply and demand more accurately than classical systems. These capabilities reduce line losses and conserve energy, while predictive modeling helps prevent issues before they arise.

Increasing Energy Efficiency of Computing Operations

One of the most compelling arguments for quantum computing is its potential to drastically reduce the energy consumption of computing operations. Today’s supercomputers consume massive amounts of electricity, but quantum systems could possibly offer a more efficient alternative.[1]

For example, the Aquila 256-qubit quantum computer uses less than 7kW of electricity—just 0.05 percent of what powerful supercomputers require.[2] Even if quantum computers handle only a fraction of supercomputing tasks, the energy savings could be substantial. Performing just 5 percent of those tasks could result in a reduction of 10GWh per year.

This enhanced efficiency is especially relevant in data processing, which is estimated to account for over 1,000TWh of global energy consumption in 2026.[3] As quantum computing becomes more capable, it could significantly reduce the environmental impact of data centers and analytics operations.

Reducing Environmental Impact of Data Processing

As the energy demands of data processing and data centers continue to skyrocket amidst efforts to reduce carbon emissions, the current trajectory is unsustainable. Advanced algorithms—especially those powering artificial intelligence (AI)—consume staggering amounts of energy. For perspective, training a single deep learning model on classical computing infrastructure can generate up to 284,000kg of CO₂,[4] which is more than the lifetime emissions of five American cars. Large language models like ChatGPT add to this footprint, producing hundreds of thousands of kilograms of CO₂ monthly. With AI adoption accelerating, the environmental impact of data processing is becoming a critical challenge.

Quantum computing offers a promising path forward. Unlike classical systems, quantum processors can perform complex calculations exponentially faster, slashing energy consumption and carbon emissions. This efficiency could transform data centers and supercomputing facilities, where power demands currently reach megawatt levels and grow by 20–40 percent annually. Quantum computing offers a way to curb this trend. By executing data processing tasks more efficiently, quantum systems can reduce both energy consumption and the associated emissions. This optimization could help make AI development more sustainable without sacrificing performance.

The Promise and the Challenge

Even with its advantages in energy efficiency, quantum computing also poses its own set of energy challenges. One of the biggest concerns is the energy required to cool quantum systems. Many quantum computers rely on cryogenic cooling, which can offset some of the efficiency gains achieved during operation. Additionally, there’s no universal standard for quantum architectures. Different systems have varying energy requirements based on their components and number of qubits. Until more systems are deployed at scale and standards are established, it is difficult to quantify the true net energy savings. Still, even with these uncertainties, quantum computing is poised to outperform classical systems in terms of sustainability. As the technology matures, its resource-saving benefits will become clearer.

Conclusion

Quantum computing holds immense potential to optimize resource use across industries, particularly in energy and data processing. While uncertainties remain—especially around cooling requirements and architectural differences—the technology is poised to make a significant impact. As quantum computing develops, it could play a pivotal role in resource optimization, including reducing the energy demand of computing operations and improving the efficiency of resource management.

[1]  https://journals.aps.org/prxenergy/abstract/10.1103/PRXEnergy.4.023008
[2] https://www.datacenterdynamics.com/en/opinions/the-dual-pronged-energy-saving-potential-of-quantum-computers/
[3] https://iea.blob.core.windows.net/assets/6b2fd954-2017-408e-bf08-952fdd62118a/Electricity2024-Analysisandforecastto2026.pdf
[4] https://arxiv.org/abs/1906.02243



« Back


Liam Critchley is a writer, journalist and communicator who specializes in chemistry and nanotechnology and how fundamental principles at the molecular level can be applied to many different application areas. Liam is perhaps best known for his informative approach and explaining complex scientific topics to both scientists and non-scientists. Liam has over 350 articles published across various scientific areas and industries that crossover with both chemistry and nanotechnology.

Liam is Senior Science Communications Officer at the Nanotechnology Industries Association (NIA) in Europe and has spent the past few years writing for companies, associations and media websites around the globe. Before becoming a writer, Liam completed master’s degrees in chemistry with nanotechnology and chemical engineering.

Aside from writing, Liam is also an advisory board member for the National Graphene Association (NGA) in the U.S., the global organization Nanotechnology World Network (NWN), and a Board of Trustees member for GlamSci–A UK-based science Charity. Liam is also a member of the British Society for Nanomedicine (BSNM) and the International Association of Advanced Materials (IAAM), as well as a peer-reviewer for multiple academic journals.


All Authors

Show More Show More
View Blogs by Date

Archives