Costa Rica - Marcar Costa Rica

Términos internacionales de comercio (Incoterms):FCA (punto de envío)
Los costos de aranceles, aduana e impuestos se cobrarán en el momento de la entrega.

Confirme su elección de moneda:

Colón costarricense
Solo se aceptan pagos con tarjetas de crédito, excepto American Express

Dólares estadounidenses
Se encuentran disponibles todas las opciones de pago

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Why PCIe 4.0 Excels in Harsh Industrial Settings Swissbit

Source: CreativeSeven/stock.adobe.com; generated with AI

By Martin Schreiber, Head of Product Management & Technical Marketing, Swissbit

As PCIe 5.0 enters the market with impressive theoretical speed gains, industrial environments often struggle to realise these benefits due to heat, power, and integration constraints. In practice, thermal limits and system design realities frequently make PCIe 4.0 and 4-channel NAND the more dependable choice for rugged applications. This blog examines why PCIe 5.0 underperforms in industrial applications, how thermal and power factors affect real-world performance, and why PCIe 4.0 paired with 4-channel architectures remains the practical standard.

In recent years, the transition from PCIe 4.0 to PCIe 5.0 has dominated discussions around high-speed interconnects in computing, especially as next-generation CPUs and motherboards become more prevalent. PCIe 5.0 promises to double the theoretical bandwidth compared to PCIe 4.0 – offering 32GT/s per lane versus 16GT/s per lane, and up to 128GB/s bidirectional throughput on a full x16 link. This leap is undeniably impressive in benchmarks and selected workloads, but the real-world impact, especially in industrial applications, remains limited due to critical environmental factors, most notably heat.

Performance Benefits: Theory vs. Practice

Lab tests and synthetic benchmarks consistently show PCIe 5.0 outperforming PCIe 4.0, particularly for sequential read/write tasks in content creation or HPC workloads. PCIe 5.0 SSDs often deliver 50–70 percent faster performance in these scenarios, with additional latency improvements from protocol and error correction enhancements.

However, in industrial deployments, these advantages are often outweighed by thermal and integration challenges:

  • Real-world industrial environments rarely allow for the cooling necessary to sustain PCIe 5.0 speeds.
  • Higher performance often leads to increased thermal output, pushing systems toward thermal throttling.
  • Advanced PCB routing and signal integrity demands raise complexity and cost.
  • Power consumption often exceeds what legacy or battery-powered systems can support.
  • Sustained high throughput is often unnecessary or unused in edge and automation applications.

Thermal Constraints in Industrial Environments

PCIe 5.0’s faster signaling introduces significantly more heat due to increased power draw and stricter signal integrity requirements. Industrial deployments typically lack the thermal headroom available in data centers, making performance throttling nearly inevitable.

Key thermal design challenges include:

  • Steep insertion loss budgets requiring active equalisation
  • More stringent PCB and connector layout constraints
  • Limited or no active airflow in compact industrial enclosures
  • High ambient operating temperatures (>40°C)
  • Space and power limits that rule out active cooling solutions

Under these constraints, many devices must reduce performance or derate their operation just to remain within safe temperature thresholds. In these cases, the theoretical speed advantage of PCIe 5.0 becomes moot. That’s why many industrial systems still favor PCIe 4.0, which offers a better balance of performance, power efficiency, and thermal stability.

NAND Channel Scaling: 4-Channel vs. 8-Channel Modules

A similar trade-off appears in NAND flash architecture. While 8-channel NAND designs theoretically double bandwidth and IOPS compared to 4-channel SSDs, the increase in complexity and heat output often leads to diminishing returns (Figure 1).

Figure 1: 8-channel SSDs show a sharp decline in performance as ambient temperature increases, whereas 4-channel SSDs maintain significantly more stable performance under rising thermal conditions. (Source: Swissbit)

Why 4-channel NAND remains preferred in industrial settings:

  • Less controller heat and reduced risk of thermal throttling
  • Lower power draw fits tighter power budgets
  • Better sustained performance in hot or unventilated environments
  • Simplified thermal design with no need for heatsinks or fans
  • Increased long-term reliability and fewer thermal-related failures

Unless advanced thermal mitigation is feasible, 4-channel modules provide a more practical and dependable solution for industrial environments.

Swissbit N3000: Thermal-Efficient Storage for Rugged Deployments

The Swissbit N3000 Series PCIe Gen4, 4-channel SSDs are purpose-built for challenging industrial environments where airflow, power, and space are constrained. With a 4-channel design that generates less heat than 8-channel SSDs, the N3000 delivers consistent, throttling-free performance even in ambient temperatures above 40°C.

Its low power consumption makes it ideal for battery-powered or remote deployments, while integrated features such as AES256 encryption, secure boot, power-fail protection, and remote management provide enterprise-grade security and data integrity. Available in compact M.2 form factors (2242/2280), it’s ideally suited for rugged systems in edge computing, robotics, automation, and telecom applications.

Balancing Performance with Practicality

In industrial applications, thermal performance and system reliability often matter more than raw speed. While PCIe 5.0 and 8-channel NAND architectures showcase compelling performance gains in theory, their practical value is often negated by real-world limitations, especially heat. Industrial integrators must prioritise long-term dependability, MTBF, and ease of integration over peak bandwidth that may not be sustained outside of lab environments.

For these reasons, technologies like PCIe 4.0 paired with 4-channel NAND remain the logical choice for most rugged deployments. They offer a stable, proven balance of performance, thermal efficiency, and reliability. Until thermal and power design innovations catch up with the speed of interface standards, newer technologies will continue to face adoption hurdles in industrial use cases.

 

Author

Martin Schreiber is Head of Product Management & Technical Marketing at Swissbit Memory Solutions. Before joining Swissbit in 2020 as a Product Marketing Manager, he spent several years in the international electronics industry, gaining experience in product management, strategy management, and design engineering.



« Back


Swissbit is a global leader in the design, development, and manufacture of flash storage and security solutions. Swissbit supplies high quality memory solutions to a wide range of markets, including industrial, embedded, communications and networking, medical equipment, and military and aerospace.


All Authors

Show More Show More
View Blogs by Date

Archives