Filtreleme seçeneklerini görmek ve aramanızı daraltmak için aşağıdan bir kategori seçin.
Sıralama Düzeni:
Sonuç Sayısına göre sıralanmış kategoriler.
Sonuçlar: 1.703
Seçin Resim Parça Numarası Ürt. Açıklama Veri Sayfası Stok Durumu Fiyatlandırma (EUR) Tablodaki sonuçları sipariş verdiğiniz miktar uyarınca birim fiyata göre filtreleyin. Miktar RoHS
SparkFun Geliştirme Kartları ve Kitleri - AVR The SparkFun Auto pHAT for Raspberry Pi is an all in one robotics package that focuses on quickly adding robot functionality and support to your Raspberry Pi or other single-board computer. The Auto pHAT can drive two small DC motors with or without 35Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Raspberry Pi Aksesuarları Raspberry Pi GPIO Ribbon Cable 40pin6 140Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Raspberry Pi Aksesuarları This 2x20 shrouded header has the same number and spacing of pins as a Raspberry Pi so you can easily connect via ribbon cable to the low-level peripherals and get hacking! This through-hole header has 40 0.1"-spaced pins and is keyed for polarity.Ch 34Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Başlıklar ve Kablo Muhafazaları This is a 2x18 pin female header. Each pin has a spacing of 0.1" in-between each other.This header mates perfectly with the Alchitry Br Prototype Element Board. 96Stokta Var
Min.: 1
Çoklu.: 1

SparkFun NFC/RFID Etiketleri ve Aktarıcıları This is a basic RFID tag that functions within the MIFARE Classic 1K guidelines. You can use these for all sorts of identification and sensing applications. The tag also has 1K of data storage which can be read and written from a compatible device. 17Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Kuvvet Sensörleri ve Yük Hücreleri This is a piezoresistive force sensor from Tekscan. The harder you press the lower the sensor's resistance. Pressing hard the resistance changes from infinite to 50k. The sensor itself is thin and flexible but the resistance does not change while 5Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Tornavidalar, Somun sürücüleri ve Soket Anahtarları What should every hacker have available to them? That's right a screwdriver (you have to get into those cases somehow). What makes screwdrivers even better is when there are a variety of interchangeable bits to use in different situations as you nee 11Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Klavyeler Multimedia Wireless Keyboard 6Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Programcı Aksesuarları This is a handy AVR programming cable that incorporates both the 10-pin and 6-pin ISP programming interfaces.Cable is about 12" long and mates with pins on 1/10in centers. 48Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Small Signal Switching Diodes This is a very common signal diode - 1N4148. Use this for signals up to 200mA of current. 107Stokta Var
Min.: 1
Çoklu.: 1
SparkFun LED Aydınlatma Geliştirme Araçları Do not look into the light. You know you want to but boy will you be sorry. 1W per channel RGB High Power LEDs in one aluminum backed package. These LEDs will blow you away. Light them up then put a coffee cup over the LED to keep your eyes from se 21Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Çok Renkli LED'ler Ever hear of a thing called RGB? Red Green Blue? How about an RGB LED? These 5mm units have four pins - one for each color and a common cathode (the longest pin). Use this LED for three status indicators or pulse width modulate all three and get mi 268Stokta Var
Min.: 1
Çoklu.: 1
SparkFun SparkFun Aksesuarları This is a tiny USB Microphone from Kinobo that plugs into your laptop desktop Raspberry Pi Jetson Nano Dev kit anything with a USB port you may be using as a computer to add microphone functionality. There is no need to install any extra software 23Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Tek Kartlı Bilgisayar Don t let the size fool you the BBC micro:bit v2 is the perfect device for you to get creative with digital technology! At half the size of a credit card this board is the ultimate tool for learning to code and building unique creations from int 14Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Antenler The TOP106 from TOPGNSS is a certified GNSS/GPS surveying antenna capable of receiving the L1/L2 bands for GPS GLONASS Galileo and BeiDou constellations. These 'UFO' antennas have incredible performance for the money. The antenna has a built in gr 4Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Basınç Sensörü Geliştirme Araçları This is a force sensitive resistor with a square 1.75x1.5" sensing area. This FSR will vary its resistance depending on how much pressure is being applied to the sensing area. The harder the force the lower the resistance. When no pressure is bein 3Stokta Var
2Beklenen 25.05.2026
Min.: 1
Çoklu.: 1

SparkFun NFC/RFID Etiketleri ve Aktarıcıları This is a simple thumbnail-size RFID tag. These tags are great for sensing presence identification etc. and they're small so they can be easily sewn into clothing or inserted into enclosures. Each tag comes with a unique 32-bit ID code and is no 24Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Kart Montajlı Sıcaklık Sensörleri PT100 Sensor 36Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Tornavidalar, Somun sürücüleri ve Soket Anahtarları This is just your basic reversible screwdriver - pocket sized! Both flat and phillips heads available. Comes with pin clip and snazzy SparkFun logo. 22Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Arayüz Geliştirme Araçları USB to RS-485 Converter

SparkFun Zigbee Modülleri - 802.15.4 After years of popularity with the XBee Series 1 and XBee Series 2 Pro Modules we now have the XBee Series 3 Pro which brings the best of both worlds. XBee 3 not only handles 802.15.4 and ZigBee but also BLE protocols and you can now talk to the m
83Stokta Var
Min.: 1
Çoklu.: 1

SparkFun Geliştirme Kartları ve Kitleri - ARM The micro:bit Educator's Lab Pack includes 10 micro:bit boards and everything you need to get you started with the new learning platform. The Lab Pack has everything you need including micro:bits cables battery packs and a few parts to experiment 5Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Sıcaklık Sensörü Geliştirme Araçları Melexis' MLX90614ESF-BAA is an infrared thermometer designed for non-contact temperature sensing. An internal 17-bit ADC and a powerful DSP contribute to the MLX90614's high accuracy and resolution. It has a huge number of applications including body 98Stokta Var
Min.: 1
Çoklu.: 1
SparkFun Anten Aksesuarları This aluminum adapter converts the very common 1/4" thread found on camera tri-pods and mono-pods to the 5/8" 11-TPI (threads per inch) found on high-end surveying antennas and equipment. It's ideal for mounting RTK surveying antennas onto a monopod 15Stokta Var
45Beklenen 24.07.2026
Min.: 1
Çoklu.: 1
SparkFun Eğitici Robotik Kitler This is the Wheel Encoder Kit from DAGU a simple add-on to any wheeled robot that can help measure the speed or distance the chassis travels. Each wheel encoder kit consists of two neodymium 8-pole magnets with rubber hubs and two hall-effect sensor 29Stokta Var
Min.: 1
Çoklu.: 1