Now at Mouser: ams AS5116 Magnetic Position Sensor for Automotive Motor Control

Yeni Ürün Basın Özeti

Bizimle İletişime Geçin


September 9, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the AS5116 on-axis magnetic position sensor from ams.

The ams AS5116 on-axis magnetic position sensor is a contactless sensor for accurate angular measurement over a full mechanical turn of 360°. This sensor features a robust architecture based on Hall sensor technology that measures the orthogonal component of the flux density (Bz) over a full-turn rotation. The AS5116 magnetic position sensor uses a simple two-pole magnet rotating over the center of the package to measure the angle. This magnet can be placed above or below the device and the absolute angle measurement provides an instant indication of the magnet's angular position. The angle information is provided by means of buffered differential sine and cosine voltages. This sensor offers high reliability, durability, low output noise, and high precision analog output. The ams AS5116 on-axis magnetic position sensor is AEC-Q100 qualified for use in automotive applications.

Applications for the ams AS5116 sensor include rotor angle sensing of electric commutated motors, electric power steering systems, electric pumps, actuators in transmission systems, starter and generator systems, and other 360° angle measurement solutions.

To learn more, visit https://www.mouser.com/new/ams/ams-as5116-hsot-magnetic-position-sensor/.