STMicroelectronics STM32WL55xx Long-Range Wireless MCUs Now at Mouser

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


STMicroelectronics STM32WL55xx Long-Range Wireless MCUs Now at Mouser

December 30, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the STM32WL55xx 32-bit wireless long-range microcontrollers from STMicroelectronics.

ST's STM32WL55xx microcontrollers embed a powerful and ultra-low-power LPWAN-compliant radio solution that allows for LoRa®, (G)FSK, (G)MSK, and BPSK modulations. The STM32WL55xx microcontrollers are are based on the high-performance Arm® Cortex®-M4 32-bit RISC core operating at a frequency of up to 48 MHz. The core implements a full set of DSP instructions and is complemented by an Arm Cortex-M0+ microcontroller. Both cores implement an independent memory protection unit (MPU) that refines the application security.

Applications for the STM32WL55xx devices include a wide range of low-power wide area network (LPWAN) wireless applications in industrial and consumer Internet of Things (IoT).

For more information, visit https://www.mouser.com/new/stmicroelectronics/stmicroelectronics-stm32wl55xx-mcus/.

About STMicroelectronics

2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology, and its products play a key role in enabling today's convergence trends.