Now at Mouser: ams OSRAM’s High-Efficiency OSLON Black Flat X LED Devices for Automotive Exterior Lighting

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


December 13, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the OSLON Black Flat X LED devices from ams OSRAM. Designed for forward lighting applications, including headlamps, night vision, and laser devices, the OSLON LED devices offer high efficiency and excellent thermal conditions. The OSLON Black Flat X LED devices have a high focus on system cost, making them a durable, cost-effective option for a wide range of lighting solutions.

The ams OSRAM OSLON 3-Chip Black Flat X KW3 HNL631.TK LEDs, available from Mouser Electronics, are high-performance light-emitting diodes offering 1350 lm at 1000 mA. The LEDs’ pad geometry offers exceptional thermal performance, allowing developers to reduce heatsink size in their lighting designs. The 3-Chip Black Flat X LEDs feature an extremely high contrast 1:200 design as a result of black case material and TiO2 casting. The OSLON 4-Chip Black Flat X KW4 HPL631.TK LEDs are an ideal replacement for halogen lamps. Offering up to 2115 lm at 1000 mA, the 4-Chip Black Flat X LEDs support a range of automotive functions, including headlamps and low-beam and high-beam applications. The devices are housed in a compact 7.59 mm × 3.75 mm × 0.50 mm package, making them a suitable choice for high-density applications.

The OSLON 5-Chip Black Flat X KW5 HQL631.TK LEDs from ams OSRAM are the most efficient lead-frame devices in the OSLON series, delivering exceptional performance in automotive exterior applications, including halogen replacement. The high-efficiency LEDs offer up to 2140 lm at 1000 mA, and they boast an operating temperature range of -40°C to +135°C.

To learn more about the ams OSRAM Black Flat X LED devices, visit https://www.mouser.com/new/ams-osram/osram-oslon-black-flat-x-devices/.

 

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.