Mouser Now Shipping ams OSRAM Mira220 Global Shutter Image Sensors for Machine Vision Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


February 15, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now shipping the Mira220 global shutter sensors from ams OSRAM. These sensors give design engineers 2D and 3D solutions for industrial machine vision applications like mobile facial authentication, smart home appliances, QR readers, AR/VR, drones, smart wearable devices, structured light vision and more.

The Mira220 2.2-megapixel global shutter image sensors support on-chip operations like external triggering, windowing, and both horizontal and vertical mirroring with an effective resolution of 1600 (H) x 1400 (V) at a maximum frame rate of 90 fps at 12-bit depth. The Mira220's advanced back-side illumination (BSI) technology stacks the sensor layer on top of the digital/readout layer. This design results in a chip-scale package with a footprint of just 5.3 mm × 5.3 mm, giving manufacturers greater freedom to optimize the design of space-constrained products such as smart glasses and VR headsets. The Mira220 also features very high sensitivity and quantum efficiency with a pixel size of 2.79 μm and is supplied in a 1/2.7” optical format.

The Mira220 features very low power consumption, with only 4 mW required in sleep mode, 40 mW in idle mode, and 350 mW at full resolution with  90 fps. By providing low system power consumption, the Mira220 enables wearable and portable device manufacturers to save space by specifying a smaller battery or extending run-time between charges. The ams OSRAM Mira220 sensors utilize the MIPI CSI-2® interface for easy interaction with processors and FPGAs, with on-chip registers that can be accessed via the standard I2C interface for easy sensor configuration. 

The ams OSRAM Mira220 global shutter image sensors are supported by the JetCis evaluation system, also available at Mouser. The JetCis evaluation system features an open development platform based on Linux running on the nVidia® Jetson Nano embedded system.

To learn more about the ams OSRAM Mira220 2.2MP global shutter image sensors, visit https://www.mouser.com/new/ams-osram/ams-osram-mira220-sensors/.

 

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.