New at Mouser: ams OSRAM Metal Can TO56 PLT5 522FA_P Green Laser Diode for Industrial and Medical Applications
April 11, 2023 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Metal Can® TO56 PLT5 522FA_P green laser diode from ams OSRAM. This device provides a highly efficient radiation source for continuous wave and pulsed operation for industrial automation, 3D sensing, and gesture recognition and is optimized for life-science applications, such as digital diagnostic devices.
The ams OSRAM Metal Can® TO56 PLT5 522FA_P green laser diode produces a 514 nm (±1 nm) typical emission wavelength with 50 mW optical output power. Featuring thermally stabilized optics in a hermetically sealed 5.6 mm diameter TO56 Metal Can package, the PLT5 522FA_P green laser diode offers high-modulation bandwidth in a single-mode semiconductor laser for reliable and maintenance-free operation.
The ams OSRAM Metal Can TO56 PLT5 522FA_P green laser diode’s excellent beam pointing accuracy and compact size improves high-density designs with better signal-to-noise ratio and optimized wavelengths. A 6 V typical operating voltage and -20°C to +60°C operating temperature range offer high performance in a low power package, providing an ideal alternative to expensive argon-ion laser devices.
Depending on the mode of operation, the PLT5 522FA_P green laser diode emits highly concentrated visible and non-visible light, which can be hazardous to the human eye. Products that incorporate this device must follow the safety precautions given in IEC 60825-1.
Applications for the PLT5 522FA_P green laser diode include confocal microscopy, spectroscopy, diagnostics for viruses, DNA sequencing and forensic analysis.
To learn more about the ams OSRAM Metal Can TO56 PLT5 522FA_P green laser diode visit https://www.mouser.com/new/ams-osram/ams-osram-plt5522fap-green-laser-diode/.
2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.
ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.