New at Mouser: ams OSRAM SPL S1L90H 1-Channel SMT Laser for Industrial LIDAR and Ranging Applications
August 10, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the SPL S1L90H 1-channel SMT laser from ams OSRAM. The SPL S1L90H SMT laser gives engineers improved performance and easier optical integration for long-distance industrial ranging and LIDAR applications, such as drones and robots, as well as building and industrial automation.
ams OSRAM's SPL S1L90H 1-channel SMT laser, available from Mouser Electronics, is a versatile, small aperture, edge-emitting laser (EEL) in a surface-mount (SMT) package with advanced chip technology. The SPL S1L90H features the highest peak power (65 W) and average power in the small package class. The device is one of the first surface-mount, edge-emitting lasers to have a 110 µm aperture, enabling a very narrow beam that is optimized for short-pulsed LiDAR applications.
The single-channel SPL S1L90H SMT Laser features ams OSRAM's multi-junction technology, consisting of three vertically stacked emitters in a single laser die mounted inside the device's 2.3 mm x 2.0 mm x 0.69 mm quad flat no-lead (QFN) package. This technology results in better target area illumination at long-range distance measurement, 3D optical sensing, and simultaneous localization and mapping (SLAM) applications.
The SPL S1L90H's optimized, power-efficient pulsed laser enables a maximum pulse width of 50 ns and is suitable for pulses shorter than 2 ns. Beam divergence is just 10° (parallel) x 25° (perpendicular), enabling efficient beam shaping with its small aperture. It is specified for corrosion robustness to class 3B, with low thermal resistance for a more straightforward system thermal design.
To learn more, visit https://www.mouser.com/new/ams-osram/ams-osram-spl-s1l90h-3-smt-laser/.
2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.
ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.