Now at Mouser: Analog Devices CN0534 LNA Receiver Reference Design for 5.8GHz ISM Applications
April 6, 2022 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the CN0534 5.8 GHz low-noise amplifier (LNA) receiver reference design from Analog Devices. The circuit provides high gain, robust overpower monitoring, and protection, all in a small footprint. This feature is an excellent addition to any 5.8 GHz ISM band application where low signal strength or distance may be a complication.
Analog Devices CN0534 LNA receiver reference design, available from Mouser Electronics, is a high-performance RF receiver system with +23 dB of gain, optimized for operation at a center frequency of 5.8 GHz. The input is unfiltered, maintaining a noise figure of 2 dB, while a bandpass filter at the output attenuates out-of-band interferers.
The CN0534 circuit includes a high-speed overpower detector and switch that protects sensitive downstream equipment connected to the receiver system. The receiver system automatically returns to regular operation when the RF power level drops within the acceptable range. The RF inputs and outputs are standard SMA connectors, and the entire design is powered from a single Micro-USB connector.
To learn more, visit https://www.mouser.com/new/analog-devices/adi-cn0534-lna-receiver-reference-design/.
2026 - Analog Devices, Inc. is a global semiconductor leader that bridges the physical and digital worlds to enable breakthroughs at the Intelligent Edge. ADI combines analog, digital, and software technologies into solutions that help drive advancements in digitized factories, mobility, and digital healthcare, combat climate change, and reliably connect humans and the world. With revenue of more than $12 billion in FY22 and approximately 25,000 people globally working alongside 125,000 global customers, ADI ensures today’s innovators stay Ahead of What’s Possible.