Apogee Semiconductor's Radiation-Hardened Low Earth Orbit A-Grade ICs, Now at Mouser, Enable Space and Medical Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


February 4, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking radiation-hardened Low Earth Orbit (LEO) A-Grade ICs from Apogee Semiconductor. These ICs include logic devices, level translators, transceivers and more. These devices are fabricated in a 180nm CMOS process utilizing proprietary radiation-hardening techniques, allowing high resiliency to single-event effects (SEE) and to a total ionizing dose (TID) up to 30krad (Si). These features make them ideal for small satellites and LEO constellations that require high performance, a small form factor and radiation resilience at a lower cost, as well as other applications where resistance to radiation is vital, such as medical imagining. These devices are also suitable for aerospace, energy, and other applications that involve harsh environments.

The Apogee Semiconductor AP54RHC288 radiation-hardened, dual-input arbiters, available from Mouser, protect critical applications by ensuring that only one output is high on each channel, regardless of the signal state at the inputs. This functionality is ideal for half-bridge drivers, thrusters, power supplies, and applications where cross-conduction must be avoided. These arbiters include a triple-redundant design throughout the circuit, which allows the devices to be immune to single-event transients (SET).

The AP54RHC86 radiation-hardened, quad 2-input XOR gates feature built-in triple redundancy for enhanced reliability and logic-level down translation to VCC. Zero-power penalty™ cold-sparing is supported, along with Class 2 ESD protection on all inputs and outputs. A proprietary output stage and robust power-on reset (POR) circuit allow the AP54RHC86 to be cold-spared in any redundant configuration with no static power loss on any pad of the device. The redundant output stage also features a high drive capability with low static power loss.

The AP54RHC04 radiation-hardened hex inverter, available to order, features proprietary cold-sparing capability with zero static power penalty and built-in triple redundancy for improved reliability. This inverter includes an internal POR circuit that ensures correct operation at voltages as low as 1.65V. The device provides logic-level down translation to VCC and supports class 2 ESD protection (4000V HBM and 500V CDM).

The AP54RHC164 radiation-hardened serial in parallel out (SIPO) shift registers include a proprietary output stage that allows for cold-sparing configurations as it avoids a leakage current penalty on inputs and outputs while in a power-down state. This feature results in considerable power savings in systems where multiple-path redundancy is employed.

To learn more about the Apogee Semiconductor's radiation-hardened ICs, visit https://www.mouser.com/manufacturer/apogee-semiconductor/.

 

Hakkında Apogee Semiconductor

2026 - Apogee Semiconductor strives to be the premier supplier of radiation hardened power, analog, and mixed signal ICs. They are rapidly growing their portfolio to provide a comprehensive suite of products, and have a team of experienced design, systems, and process engineers who are taking a different approach to radiation hardened by design (RHBD) IC design.