Digi ConnectCore 93 System-On-Module, Now Available at Mouser, Supports Longevity and Scalability for Industrial IoT Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Learn more about the ConnectCore 93 SOM

December 5, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the ConnectCore® 93 system-on-module (SOM) from Digi. Based on the industrial NXP Semiconductors i.MX 93 applications processor, the ConnectCore 93 SOM is designed for a wide range of Internet of Things (IoT) devices for medical, industrial, energy, and transportation. The new SOM is an ideal choice for automation, human-machine interfaces, equipment monitoring, edge computing, and machine learning applications.

The Digi ConnectCore 93 SOM, now available at Mouser, features up to two Arm® Cortex®-A55 cores, while a Cortex-M33 core, AI/ML Arm Ethos U65 NPU and NXP PMIC ensure maximum power efficiency. The SOM features pre-certified dual-band 802.11ax Wi-Fi 6 and Bluetooth® 5.3 connectivity, as well as seamless cellular modem and Digi XBee® integration. Housed in a surface-mount, 40 mm x 45 mm form factor, the ConnectCore 93 SOM is designed to deliver industrial reliability for embedded devices. The new SOM also offers exceptional security and privacy with Digi TrustFence®, a fully integrated device security framework that simplifies the process of securing connected devices. The ConnectCore 93 SOM supports an industrial operating temperature range of -40 °C to +85 °C, in addition to product lifecycles of 10+ years for embedded devices. This SOM is designed for industrial reliability and 10+ year product lifecycles of embedded devices. The Digi SMTplus® surface-mount form factor provides simplified design integration, efficiency and reliability.

The ConnectCore 93 SOM is supported by the ConnectCore 93 development kit. This comprehensive demonstration platform includes a development board and an i.MX 93 dual-core, NPU, 8 GBytes eMMC, and 1 GByte LPDDR4 wireless SOM. The development kit also includes reference designs and online documentation, allowing designers to quickly prototype and scale industrial IoT applications.

To learn more about the ConnectCore 93 SOM, visit https://www.mouser.com/new/digi-international/digi-connectcore-93-soms/.

 

Hakkında Digi

2026 - Digi International (Digi) is a leading global provider of mission-critical machine-to-machine (M2M) and Internet of Things (IoT) connectivity products and services. The company helps its customers create next-generation connected products and deploy and manage critical communications infrastructures. Founded in 1985, Digi has helped customers connect over 100 million things, and growing.