New at Mouser: Espressif Systems ESP32-C61 Wi-Fi 6 + Bluetooth 5 (LE) SoC for IoT, Industrial, Robotics, and Smart Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Learn more about the ESP32-C61 SoC
Learn more about the ESP32-C61 SoC

February 9, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new ESP32-C61 Wi-Fi® 6 + Bluetooth® 5 (LE) System-on-Chip (SoC) from Espressif Systems. The ESP32-C61 SoC is designed for IoT, smart home, industrial, robotics, sensor, and medical device applications.

The Espressif Systems ESP32-C61 SoC, available from Mouser, features optimized peripherals and improved connectivity, powered by a 32-bit RISC-V processor running at up to 160 MHz, including external PSRAM support. This enables developers to build feature-rich applications, allowing for larger data buffers, additional functionality, and future upgrades with less time spent on memory optimization. The ESP32-C61 supports a 20MHz bandwidth for 802.11ax mode and a 20MHz/40MHz bandwidth for 802.11b/g/n mode, featuring characteristics, such as OFDMA and MU-MIMO for reliable and low-latency connections, as well asl target wake time (TWT) for ultra-low power applications. Additionally, the ESP32-C61 chip incorporates a robust set of peripherals, including SPI, I2C, UART, I2S, ADC, GDMA, ETM, and an analog comparator. The Bluetooth 5 (LE) radio enables long-range operation via advertisement extension and a coded PHY, while supporting a high-throughput PHY of 2 Mbps. The ESP32-C61 also supports the BLE Mesh 1.1 protocol, ESP-IDF, and the ESP-Matter SDK, or can operate as a wireless co-processor through ESP-AT or ESP-Hosted, facilitating seamless integration into various system architectures.

The ESP32-C61 features secure boot, flash, and PSRAM encryption with cryptographic accelerators and has an ECDSA-based digital signature peripheral (DSP) in hardware, thus safeguarding private keys from software access. The addition of a trusted execution environment (TEE), utilizing access permission management (APM), a hardware block, and physical memory protection (PMP), provides mechanisms for software isolation.

To learn more, visit https://www.mouser.com/new/espressif/espressif-esp32-c61-socs/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

About Espressif Systems

2026 - Espressif Systems is an advanced and professional IC design company that provides low-power Wi-Fi and Bluetooth SoCs and wireless solutions for Internet of Things (IoT) applications. The company has a team of innovators from around the world, working in the areas of chip design, algorithm research, software development, open source development, product development, and customer services.