Mouser-Backed Formula E Team Kicks Off Season 9 in Mexico City

Hemen Yayınlanması İçin

Bizimle İletişime Geçin


Mouser Formula E landing page
Stoffel Vandoorne and Jean-Éric Vergne

January 04, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, cheers on the DS PENSKE Formula E team as they kick off Season 9 at the Autodromo Hermanos Rodriguez track in Mexico City on January 14, 2023. With a race-ready surface and long corners, Mexico City is one of the fastest tracks on the calendar, featuring a mix of long and fast straights and a technical infield section through Foro Sol stadium. Mouser is partnering with the DS PENSKE team throughout the 2022–23 ABB FIA Formula E World Championship racing season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX.

The DS PENSKE team will be racing the new third-generation Formula E DS E-TENSE FE23, which combines high-performance, efficiency, and stability. The Gen3 cars feature a top speed of 280 kph, are 60 kg lighter than the Gen2 cars, and offer double the regen capacity — meaning more than 40% of the energy used in-race is via regeneration under braking.

The team benefits from two past Formula E Champions driving its cars, the reigning World Champion Stoffel Vandoorne and the two-time Formula E Champion, Jean-Éric Vergne. In the time trials leading up to the race, Jean-Éric Vergne fired DS PENSKE to the top of the timesheets, setting the fastest time of the week with a new benchmark of 1:25.248.

The Formula E series features cars powered solely by electricity and represents a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more, visit https://www.mouser.com/formula-e/.