TDK InvenSense IIM-20670 MotionTracking MEMS Device, Now Available at Mouser, Supports Industrial, Drone, and Robotics Applications
January 11, 2024 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the IIM-20670 MotionTracking® MEMS device from TDK InvenSense. The IIM-20670 is a robust SmartIndustrial™ 6-axis inertial measurement unit (IMU) for tilt and stabilization applications. The device supports industrial applications requiring extreme stability over temperature and strong immunity to vibration. The IIM-20670 is an ideal choice for industrial automation, 5G platforms, robotics, and industrial and agricultural drones.
The TDK InvenSense IIM-20670 device, now available at Mouser, consists of a monolithic 6-axis IMU, a 3-axis accelerometer, and a 3-axis gyroscope. The IIM-20670 offers impressive shock robustness, as well as the ability to measure all six axes simultaneously while maintaining current consumption below 10 mA under all operating conditions. The IIM-20670 device features programmable digital filters and a 10 MHz SPI interface capable of assessing data integrity using a CRC-based error-detecting code algorithm.
The IIM-20670 MotionTracking MEMS device offers an accelerometer thermal stability of 1.7 µg/C, accelerometer bias repeatability of 1 mg, and a programmable output of 64 G. The new MEMS device is RoHS and Green compliant and is housed in a compact 4.5 mm x 4.5 mm x 1.1 mm DQFN package, ideal for space-constrained applications.
The DK-20670 development kit, also available from Mouser, is a demonstration and evaluation platform for the IIM-20670 MotionTracking MEMS device. The DK-20670 development kit provides an example application circuit, allowing rapid prototyping when incorporated into existing designs.
To learn more about the InvenSense IIM-20670 MotionTracking MEMS device, visit https://www.mouser.com/new/tdk/tdk-iim-20670-motiontracking-device/.
2026 - InvenSense, Inc., a TDK Group company, is a world-leading provider of MEMS sensor platforms. InvenSense's vision of Sensing Everything® targets the consumer electronics and industrial areas with integrated motion and sound solutions. InvenSense solutions combine MEMS (micro electrical mechanical systems) sensors, such as accelerometers, gyroscopes, compasses, and microphones, with proprietary algorithms and firmware that intelligently process, synthesize, and calibrate the output of sensors, maximizing performance and accuracy. InvenSense's motion tracking, audio and location platforms, and services can be found in mobile, wearables, smart home, industrial, automotive, and IoT products. In May of 2017, InvenSense became part of the MEMS Sensors Business Group within the newly formed Sensor Systems Business Company of TDK Corporation. InvenSense is headquartered in San Jose, California, and has offices worldwide.