New at Mouser: Microchip Technology's PIC16F13145 Microcontroller with the Configurable Logic Block

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


April 1, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the PIC16F13145 family of microcontrollers from Microchip Technology.

The PIC16F13145 microcontroller family introduces the Configurable Logic Block (CLB) peripheral, enabling users to incorporate hardware-based custom logic into their applications. Building on over a decade of experience with the Configurable Logic Cell (CLC), Microchip has now evolved its customizable logic offering with the CLB to enable even more complex hardware-based functions. The CLB performs custom hardware-based digital logic independently of the CPU, improving response time and power consumption. Users can configure the basic logic elements as matrix multipliers, look up tables, and flip-flops to achieve logic functions.

The PIC16F13145 microcontrollers also include other Core Independent Peripherals (CIPs), including a 10-bit analog-to-digital converter with computation (ADCC), an 8-bit digital-to-analog converter (DAC), two rapid comparators with a 50 ns response time, 8- and 16-bit timers and I2C/SPI communication modules. These microcontrollers are offered in package sizes from 8 to 20 pins for design flexibility while also helping eliminate the need for external logic components and reducing BOM cost and power consumption.

The PIC16F13145 family of MCUs is supported by the PIC16F13145 Curiosity Nano evaluation kit (EV06M52A), also available from Mouser. The evaluation kit's integrated programmer/debugger eliminates the need for external tools, and Microchip's free-to-use MPLAB® X IDE and MPLAB Code Configurator (MCC) provides an easy GUI-based interface to configure the device and all on-board peripherals, including the CLB.

Mouser, in partnership with Microchip and All About Circuits, is currently sponsoring the 2025 Configurable Logic Design Challenge, a fantastic opportunity for developers to showcase their skills and creativity using the innovative Configurable Logic Block (CLB) peripheral. To enter, users need to submit an abstract outlining an innovative application for the PIC16F13145 MCU. If the abstract is approved, they will receive a free PIC16F13145 Curiosity Nano evaluation kit to build their design. With cutting-edge logic technology, expert judges, complimentary development tools and a total prize pool of $10,000, the possibilities are endless. To learn more about the 2025 Configurable Logic Design Challenge, visit https://www.allaboutcircuits.com/giveaways/pic16f13145/.

To learn more about the PIC16F13145 Microcontrollers, visit https://www.mouser.com/new/microchip/microchip-pic16f13145-microcontrollers/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.