Morse Micro's HaLowLink 2 Long Range Sub-1 GHz Wi-Fi Gateway, Now at Mouser, Delivers Top-Notch Wireless Range and Performance
April 14, 2026 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the HaLowLink 2 long-range sub-1 GHz Wi-Fi® gateway from Morse Micro. The HaLowLink 2 is an all-in-one Wi-Fi HaLow router, access point, and extender designed to unlock the full potential of Morse Micro's Wi-Fi HaLow technology. Powered by Morse Micro's newest and highest-performing chipset, the HaLowLink 2 is ideal for large-scale Internet of Things (IoT) deployment and expansive environments such as smart cities, industrial and commercial campuses, and agriculture.
The Morse Micro HaLowLink 2 gateway, now at Mouser, features the MM8108 Wi-Fi HaLow System-on-Chip (SoC), which delivers 43 Mbps throughput at extended range. The HaLowLink 2 can be deployed as a router, access point, and extender to create a network optimized for HaLow devices. When paired with a second HaLowLink 2, it creates 2.4 GHz Wi-Fi hotspots beyond the reach of traditional Wi-Fi, enabling robust connectivity for non-HaLow devices. Users can connect up to 1,000 IoT end devices with the HaLowLink 2 gateway, and the Sub-1 GHz signal penetrates multiple floors and walls.
The HaLow 2 simplifies deployment and improves performance across regions worldwide, including the US, Canada, Australia, the UK, Europe, and Japan, and includes region-specific antennas and power adapters. The HaLowLink 2 long-range gateway features an intuitive industrial design and plug-and-play connectivity.
To learn more, visit https://www.mouser.com/new/morse-micro/morse-micro-halowlink-2-gateways/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
2026 - Morse Micro builds a new generation of wireless chips that reach farther, are lower power, and are genuinely secure. The company is a dedicated contributor to the Wi-Fi Alliance's efforts to bring interoperability certifications for Wi-Fi HaLow technology to the market. Morse Micro serves commercial, residential, and industrial IoT markets, with applications including access control, security cameras, industrial automation, and retail and mobile devices. The company's turnkey solutions enable a wide range of smart devices to connect wirelessly.