Morse Micro MM8108 SoC, Now at Mouser, Delivers Next Generation Wi-Fi HaLow Performance for IoT Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Learn more about the MM8108 SoC
Learn more about the MM8108 SoC

December 10, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new MM8108 Wi-Fi® HaLow® System-on-chip (SoC) from Morse Micro. The MM8108 SoC is a HaLow-compliant connectivity solution tailored to meet the needs of Internet of Things (IoT) and machine-to-machine (M2M) applications.

The Morse Micro MM8108 SoC, available from Mouser, is a highly integrated, ultra-low-power, single-chip Wi-Fi solution offering improved performance in all key areas, including range, throughput, and power efficiency, while also reducing the cost, effort, and time required to bring the next generation of Wi-Fi HaLow-enabled products to market. Wi-Fi HaLow is the first Wi-Fi standard tailored to meet the needs of IoT applications, and the MM8108 delivers over-the-air data rates up to 43.33Mbps at 8MHz bandwidth in worldwide sub-GHz license-exempt bands, with next-generation upgrades boasting 16x better efficiency than standard Wi-Fi. The MM8108 adds an integrated high-efficiency power amplifier (PA) and high-linearity low-noise amplifier (LNA) that meet the IEEE 802.11ah standard, while integrating full MAC and PHY implementations. The MM8108's RF interface can also be configured with an external PCB-mount PA or front-end module (FEM) for ultra-long-reach applications with leading Wi-Fi HaLow security features (WPA3, SAE, GCMP) to ensure link-layer communications start and remain protected.

Mouser also stocks several evaluation kits for the MM8108 SoC. The Morse Micro MM8108-EKH01-01 kits offer a prototyping platform based on the Raspberry Pi 4B. These fully enclosed kits provide out-of-the-box Wi-Fi HaLow connectivity for low-power, long-range wireless IoT applications. The MM8108-EKH05-01 evaluation kit is a fully integrated development platform for a wide range of IoT applications featuring an MM8108 SoC, an STM32U585 low-power microcontroller (MCU), and a BlueNRG-M2 Bluetooth® SoC. The MM8108-EKH19 kit features a USB 2.0 network adapter reference design based on the MM8108 SoC, an SMA Wi-Fi HaLow antenna, and a GL-MT3000 router.

To learn more about the MM8108 SoC, visit: https://www.mouser.com/new/morse-micro/morse-micro-mm8108-soc/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

About Morse Micro

2026 - Morse Micro builds a new generation of wireless chips that reach farther, are lower power, and are genuinely secure. The company is a dedicated contributor to the Wi-Fi Alliance's efforts to bring interoperability certifications for Wi-Fi HaLow technology to the market. Morse Micro serves commercial, residential, and industrial IoT markets, with applications including access control, security cameras, industrial automation, and retail and mobile devices. The company's turn-key solution enables a whole new range of smart devices to connect wirelessly.