Murata's New Type 2AB Ultra-Wideband Module, Now at Mouser, Delivers Exceptional Performance for Size- and Power-Sensitive Applications
Month 23, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the Type 2AB UWB+BLE combo ultra-wideband module from Murata Electronics, featuring both ultra-wideband (UWB) (channels 5 and 9) and Bluetooth® Low Energy (BLE) 5.2 RF technology. Offering low current consumption and a small form factor, the combo module supports a range of small, battery-operated applications, including Internet of Things (IoT) devices, connected tracking devices, industrial sensors and controllers, and condition monitoring solutions.
The Murata Type 2AB UWB+BLE ultra-wideband module, now available at Mouser, delivers an exceptional battery life of more than ten years in an ultra-small, 10.5 mm × 83 mm × 1.44 mm package. The module features an embedded reference clock and an integrated three-axis sensor, while sophisticated collaborative coexistence hardware mechanisms and algorithms ensure that WLAN and Bluetooth collaboration is optimized for maximum performance. The high-performance module is based on the NXP 88W9098 combo chipset, supporting Wi-Fi® 6 (802.11a/b/g/n/ac/ax) 2×2 MIMO and Bluetooth 5.3 BR/EDR/LE 2MPHY up to a 1200 Mbps PHY data rate on Wi-Fi and a 3Mbps PHY data rate on Bluetooth. The module's WLAN section supports the PCIe 2.0 interface with optional support for SDIO 3.0, while the Bluetooth section supports the high-speed four-wire UART interface and PCM for audio data.
The Type 2AB UWB+BLE module's low-power performance and small form factor make it an ideal choice for size- and power-sensitive applications, including handheld wireless systems, gateways, and video streaming solutions.
The Type 2AB UWB+BLE module is supported by the LBUA5QJ2AB-828EVB evaluation kit. The evaluation kit offers a complete test and development platform on a 47 mm × 80 mm PCB, with a pre-mounted Type 2AB module, onboard UWB and BLE antennas and all required support circuitry. USB Type-C™ connectors enable easy connection to power and a PC.
To learn more about the Type 2AB UWB+BLE combo ultra-wideband module, visit https://www.mouser.com/new/murata/murata-type-2ab-module/.
2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations are used in a wide range of applications, including mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan "Innovator in Electronics®," approximately 48,000 Murata employees strive every day to develop promising new technologies, "world's first" innovations, and products shaping the future of electronics, all to enable customers to realize their vision.