Murata Electronics Type 2FP Wi-Fi 6 + Bluetooth LE Multi-Radio Module, Now at Mouser, Provides Advanced Security and Radio Capabilities
February 26, 2026 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the new Type 2FP Wi-Fi® 6 + Bluetooth® Low Energy (LE) 5.4 multi-radio module from Murata Electronics. The compact, highly integrated Type 2FP module is based on the NXP RW610 wireless microcontroller (MCU). The built-in, high-performance MCU provides advanced security features for connected smart devices in smart homes, enterprise and industrial automation, smart accessories, and smart energy applications.
The Murata Electronics Type 2FP module, now at Mouser, supports dual-band Wi-Fi 6, Bluetooth LE 5.4, and Ethernet to ensure seamless connectivity and operational efficiency. The Type 2FP module also supports the latest Matter smart home connectivity protocol over Wi-Fi, Thread, and Ethernet, simplifying device interoperability and management.
The Type 2FP multi-radio module features 1.2 MB of SRAM, 16 MB of Flash, and an external PSRAM interface for system memory expansion up to 128 MB. The modules support a total of 64 GPIOs and rich peripheral interfaces, including FlexComm interfaces, SDIO 3.0, high-speed USB 2.0 On-The-Go (OTG) with integrated PHY, and digital microphone support. The built-in RW610 Wireless MCU provides advanced security features such as NXP EdgeLock™ Assurance, NXP EdgeLock 2GO Trust Provisioning, a trusted execution environment (TEE) based on Arm TrustZone-Mand, and hardware root of trust. The surface-mount type modules measure just 12 x 11 x 1.5 mm and weigh 0.54 g. The Type 2FP Wi-Fi 6+ module meets the Moisture Sensitivity Level (MSL) 3 standard and operates over a temperature range of -40°C to 85°C.
To learn more, visit https://www.mouser.com/new/murata/murata-type-2fp-radio-modules/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations can be found in a wide range of applications: mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan, “Innovator in Electronics®,” approximately 48,000 Murata employees strive every day to develop promising new technologies, “world’s first” innovations, and products shaping the future of electronics, all toward enabling customers to realize their vision.