Murata Type 2LL Wi-Fi 6/Bluetooth/802.15.4 Module, Now at Mouser, Enables IoT, Wireless, and Gateway Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Learn more about the Type 2LL module
Learn more about the Type 2LL module

June 11, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new ultra-compact Type 2LL Wi-Fi® 6/Bluetooth®/802.15.4 module from Murata. The Type 2LL module is a small, high-performance solution designed to enhance connectivity and efficiency in various IoT, handheld wireless, and gateway applications.

The Murata Type 2LL module, available from Mouser, is based on the IW610G tri-radio system-on-chip (SoC)  from NXP® Semiconductors, which integrates Wi-Fi 6, Bluetooth Low Energy (BLE) 5.4, and 802.15.4 radios into a compact solution, providing robust wireless communication capabilities.

The Wi-Fi 6 subsystem offers improved network efficiency, reduced latency, and an extended range, while the Bluetooth LE radio supports high-speed data rates and long-range communication. Additionally, the 802.15.4 radio offers PHY data rates of up to 114.7 Mbps on Wi-Fi and 2 Mbps on BLE. The Wi-Fi supports SDIO v3.0 DDR50 interfaces, while the Bluetooth section facilitates a high-speed 4-wire UART interface and PCM for audio data.

The Type 2LL module is packaged in an impressively small, shielded form factor (8.8 × 7.7 × 1.3 mm3) that facilitates integration into size and power-sensitive applications. The Type 2LL employs highly rich, enhanced collaborative coexistence hardware mechanisms and algorithms, enabling optimized collaboration among Wi-Fi, Bluetooth, and 802.15.4 for maximum performance. In IEEE 802.11ax mode, the Wi-Fi operation assists rates of MCS0-MCS9 (up to 256QAM) in 20MHz channels for data rates.

To learn more, visit https://www.mouser.com/new/murata/murata-type-2ll-module/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

About Murata

2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations are used in a wide range of applications, including mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan "Innovator in Electronics®," approximately 48,000 Murata employees strive every day to develop promising new technologies, "world's first" innovations, and products shaping the future of electronics, all to enable customers to realize their vision.