Mouser Now Shipping the Murata Type 2BZ Wi-Fi + Bluetooth Module for IoT and Handheld Wireless Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


May 2, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Type 2BZ Wi-Fi® + Bluetooth® module (LBEE5XV2BZ) from Murata. The Type 2BZ Wi-Fi + Bluetooth module provides engineers with a dual-band, small form-factor wireless connectivity solution for power-sensitive applications like the Internet of Things (IoT), handheld wireless, gateways, Smart Home and industrial applications, to name a few.

The Murata Type 2BZ Wi-Fi + Bluetooth module, available from Mouser Electronics, is a small, high-performance wireless connectivity module based on the Infineon CYW54590 combo chipset. Featuring highly sophisticated, enhanced collaborative co-existence hardware mechanisms and algorithms, the Type 2BZ module ensures that wireless local area network (WLAN) and Bluetooth collaboration is optimized for maximum performance, with up to 866 Mbps PHY (physical) data rate on Wi-Fi and 3 Mbps PHY data rate on Bluetooth.

The Type 2BZ module’s WLAN section supports secure digital input output (SDIO) v3.0 interface, while the Bluetooth section supports a high-speed 4-wire universal asynchronous receiver/transmitter (UART) interface and pulse-code modulation (PCM) for audio data. In IEEE 802.11ac mode, the WLAN operation provides rates up to 256 quadrature amplitude modulation (QAM) in 20 MHz, 40 MHz, and 80 MHz channels, supporting Wi-Fi 802.11a/b/g/n/ac with 2×2 multiple input multiple output (MIMO) + 5.2 BR/EDR/LE (Bluetooth basic rate/enhanced data rate/low energy). This comes packaged in an impressively small form factor for size- and power-sensitive industrial applications, with operating temperatures up to +85°C.

To learn more about the new Type 2BZ Wi-Fi + Bluetooth module from Murata, visit https://www.mouser.com/new/murata/murata-type2bz-wifi-bluetooth-module/.

 

About Murata

2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations are used in a wide range of applications, including mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan "Innovator in Electronics®," approximately 48,000 Murata employees strive every day to develop promising new technologies, "world's first" innovations, and products shaping the future of electronics, all to enable customers to realize their vision.