Nexperia’s NEH2000BYJ PMIC, Now Available at Mouser, Offers High-Performance Energy Harvesting for Low-Power Applications
April 25, 2023 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now stocking the NEH2000BYJ energy harvesting power management integrated circuit (PMIC) from Nexperia. The NEH2000BYJ PMIC harvests energy generated by a photovoltaic (PV) cell, which in turn charges a rechargeable battery. The new PMIC from Nexperia is an ideal choice for low-power applications, including wireless Internet of Things (IoT) devices, wearable devices, smart remote controls, and industrial and environmental monitoring.
The Nexperia NEH2000BYJ energy harvesting PMIC, now available at Mouser, includes pre-sets on the chip, making the implementation of energy harvesting designs simpler. This offers an unprecedented ease-of-use for engineers. Even with limited energy harvesting knowledge, it is possible to quickly integrate and deploy high-performing energy harvesting in new product designs.
Nexperia’s advanced maximum power point tracking (MPPT) uses an embedded hill-climbing algorithm to deliver the maximum power to the load. The MPPT is designed to be independent of specific characteristics of the harvesters, therefore any harvester that fits the specifications of the chip can be used. In addition, the MPPT circuit can detect the maximum power point with an interval of 0.7 seconds resulting in maximum efficiency in various environments where energy can rapidly change over time. The MPPT functions autonomously and requires no pre-programming. Consequently, self-optimization makes it no longer required to have an extremely detailed understanding of the fluctuating environment.
The NEH2000BYJ PMIC offers a harvesting power range from 35 μW to 2 mW and is available in a compact, 16-lead 3.0 mm × 3.0 mm QFN package, ideal for space-constrained applications.
To learn more about the NEH2000BYJ energy harvesting PMIC from Nexperia, visit https://www.mouser.com/new/nexperia/nexperia-neh2000byj-pmic/.
2026 - Nexperia, headquartered in the Netherlands, is a global semiconductor company with a rich European history and over 12,500 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.