Mouser Now Stocking New Omron Electronics E8Y-L Micropressure Sensors for Industrial Automation

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Learn more about the E8YL micropressure sensors
Learn more about the E8YL micropressure sensors

January 21, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new E8Y-L micropressure sensors with digital display from Omron Electronics. The E8Y-L devices are compact digital pressure sensors designed to save space and provide clear on-site monitoring for industrial manufacturing equipment and factory automation applications.

The Omron E8Y-L micropressure sensors feature a compact design (31mm × 30mm × 30mm) and an easy-to-read red LED indicator, enabling the monitoring of pressure in various scenarios and different zones. This allows applications such as maintaining regulated pressure in a clean room or automatically regulating ducts or valves. These EN- and UL-approved sensors include analog current output models and pressure port Rc (PT) 1/8 models offering zero-point adjustment, and automatic teaching settings that allow users to set custom pressures at which the sensor turns on or off. Users can set the zero point to any value to simplify tracking pressure changes in semiconductor wafer-processing reactors, monitoring organic gas flow paths during implantation, or in safety systems such as purge gas leakage detection. In addition, users can interact with the device via four simple buttons on the front panel to select the measurement range, displayed channel, operating mode, or set thresholds for the upper and lower limits of measurement pressure, which can simplify the detection of machinery faults, such as clogged exhausts or blocked vents.

The E8Y-L sensors operate from -10°C to 55°C, with no condensation or icing, and can withstand up to 85% relative humidity, making them suitable for use in a wide variety of industrial environments. With a wide supply voltage range of 12V to 24V and a current consumption of up to 50mA or 75mA, the sensors are ready to operate from popular industrial power rails. The E8Y-L sensors were featured in a recent Mouser "New Tech Tuesday" blog.

To learn more about the E8YL micropressure sensors, visit https://www.mouser.com/new/omron-electronics/omron-e8y-l-micropressure-sensors/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

About Omron

2026 - Omron is a world leading supplier of technologically advanced electronic components. Omron's vast product line includes switches (general, snap-action, control, DIP/SIP, miniature, sub-miniature, and thumbwheel), relays, connectors, optoelectronics, and sensors that are used in consumer electronics, computer peripherals, office automation products, and telecom applications. Omron Industrial Automation supplies the world with advanced electronics and control system components, including switches, relays, power supplies, sensors, calibration equipment, and cable assemblies. Omron is a global leader in RFID technology with their extensive range of reliable products and systems, such as inlays, readers/writers, transponders, development tools, and accessories.