New at Mouser: onsemi Acuros CQD SWIR Cameras for AI, Industrial, Automotive, Agricultural and Medical Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


March 19, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping Acuros® CQD® shortwave infrared (SWIR) cameras from onsemi. The Acuros CQD cameras provide high-resolution imaging and sensing capabilities across the visible, near-infrared (NIR), and shortwave infrared (SWIR) spectrum for machine vision, security, industrial, thermography, automotive, agricultural, and medical imaging.

The onsemi Acuros CQD cameras, available from Mouser, feature 400nm to 1,700nm broadband image sensor technology based on colloidal quantum dot (CQD) thin film photodiodes fabricated monolithically on silicon readout wafers. The cameras offer high frame rates, global shutter operation, and up to 70dB of dynamic range. The Acuros CQD cameras are available in a variety of Acuros sensor sizes, including a 6.3 megapixel (MP) (3064 x 2040), 4.2 MP (2040 x 2040), 2.1 MP (1920 x 1080), 1.2 MP (1280 x 1024), or VGA (640 x 512) format sensor. The camera includes USB3 Vision, GigE Vision and CameraLink interfaces to provide end users the flexibility of programmable frame time, exposure time, gain modes, window modes, binning modes, and more.

Designed for use in multi-tool imaging systems, the Acuros CQD cameras are compatible with a wide range of SWIR lenses and can be operated by an internal clock or externally triggered via software or a hardware TTL trigger input. The Acuros CQD cameras have EAR-99 export classification, which requires no license for global export. This makes the Acuros CQD the ideal choice for integration in both multi-national and domestic supply chains and manufacturing operations.

To learn more, visit https://www.mouser.com/new/onsemi/onsemi-acuros-swir-cameras/.

 

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.