Now at Mouser: Raspberry Pi's Hailo 8L AI Kit for Complex AI Vision Applications

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


December 9, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the Hailo 8L AI kit from Raspberry Pi. The AI kit, which combines the pre-installed Raspberry Pi M.2 HAT+ with an M.2-format Hailo 8L AI accelerator, is ready to use out of the box. The Hailo 8L AI kit provides a cost-effective and power-efficient way to integrate high-performance artificial intelligence (AI) in applications, including process control, security, home automation, voice recognition, and robotics.  

The Raspberry Pi Hailo 8L AI kit, now available at Mouser, is a 13 tera-operations per second (TOPS) neural network inference accelerator built around the Hailo 8L chip. When installed on a Raspberry Pi 5, the kit allows users to quickly create complex AI vision applications with low latency and minimal power requirements. Neural networks for facial landmarking, instance segmentation, object detection, and other tasks run entirely on the Hailo 8L module, leaving the Raspberry Pi 5's CPU free to handle different processes. A thermal pad, pre-fitted between the module and the HAT+, spreads heat across components to improve performance and ensure consistent operation.

The Hailo 8L AI Kit includes a 16mm stacking header, spacers, and screws for easy installation in a Raspberry Pi 5 with the Raspberry Pi Active Cooler in place. Fully integrated into Raspberry Pi's camera software stack, the kit simplifies image processing for real-world, AI-based vision applications. The Hailo 8L AI Kit meets Raspberry Pi's HAT+ specification and has an operating temperature range of 0℃ to 50℃.

To learn more, visit https://www.mouser.com/new/raspberry-pi/raspberry-pi-hailo-8l-ai-kit/.

 

About Raspberry Pi

2026 - Raspberry Pi Ltd makes computing accessible to people and businesses all over the world. Low-cost, high-quality, compact and efficient, Raspberry Pi products are used everywhere, from home computing to factory control, from retro gaming to embedded applications, and from education to enterprise. Since selling their first product in 2012, they've become the UK's bestselling computer company.