Mouser Electronics Now Stocking Silicon Labs' xG28 Family of SoCs for Long-Range Applications at the Edge
November 6, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the FG28 system-on-chip (SoC) from Silicon Labs. The FG28 is designed for long-range networks and protocols like Amazon Sidewalk, Wi-SUN, and other proprietary protocols.
The FG28, available from Mouser, is a dual-band SoC including radios for sub-Gigahertz (GHz) and 2.4 GHz Bluetooth® LE, as well as a built-in AI/ML accelerator for machine learning inference, and Silicon Labs' industry-leading Secure Vault™ technology.
Also available from Mouser is Silicon Lab's new ZG28, a Z-Wave Long Range SoC; the SG28, an Amazon Sidewalk SoC; and the PG28, a stand-alone microcontroller. These devices all feature a 32-bit Arm® Cortex®-M33 core with an 80 MHz maximum operating frequency and rich analog and communication peripherals.
The xG28 family of wireless SoCs combine Bluetooth connectivity, giving users an easy way to provision and deploy new devices onto the network, with a sub-GHz band designed to support device communications over one mile, allowing for new edge applications in areas like smart agriculture, smart cities, and neighborhood networks like Amazon Sidewalk.
The xG28 family of wireless SoCs are supported by the xG28-EK2705A 900 MHz BLE Explorer Kit, the xG28-PK6025A 868-915 MHz BLE Pro-Kit, and the xG28-PK6024A 868-915 MHz BLE +14-dBm Pro-Kit. Each kit includes a main board with an onboard J-Link debugger with a Packet Trace Interface and a Virtual COM port. The kits also include a radio board that provides a complete reference design for the xG28 Wireless SoCs. The main board enables application development and debugging of the attached radio board and external hardware through an expansion header. The Silicon Labs xG28 Explorer Kit and Pro-Kits provide all the necessary tools for developing high-volume, scalable Sub-GHz + 2.4 BLE wireless IoT applications.
To learn more about the FG28 dual-band SoC, visit https://www.mouser.com/new/silicon-labs/silicon-labs-fg28-dual-band-soc/.
To learn more about the ZG28 Z-Wave Long Range SoC, visit https://www.mouser.com/new/silicon-labs/silicon-labs-efr32zg28-z-wave-soc/.
To learn more about the SG28 Amazon Sidewalk SoC, visit https://www.mouser.com/new/silicon-labs/silicon-labs-efr32sg28-dual-band-socs/.
To learn more about the PG28 stand-alone microcontroller, visit https://www.mouser.com/new/silicon-labs/silicon-labs-efm32pg28-general-purpose-mcus/.
2026 - Silicon Labs is a leading innovator in low-power wireless connectivity, building embedded technology that connects devices and improves lives. Merging cutting-edge technology into the world’s most highly integrated SoCs, Silicon Labs provides device makers with the solutions, support, and ecosystems needed to create advanced edge connectivity applications. Headquartered in Austin, Texas, Silicon Labs has operations in over 16 countries and is the trusted partner for innovative solutions in the smart home, industrial IoT, and smart cities markets.