STMicroelectronics' New LSM6DSV16BX Motion and Bone-Conduction Sensor, Now at Mouser, Offers Superior Performance in Hearable Devices and Headsets

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


March 27, 2023Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the LSM6DSV16BX motion and bone-conduction sensor from STMicroelectronics. Combining a three-axis digital accelerometer and three-axis digital gyroscope, the LSM6DSV16BX sensor provides advanced functions for applications including wearable and hearable devices, motion tracking and gesture detection, Internet of Things (IoT) and connected devices, and bone conduction for vibration detection.

The STMicroelectronics LSM6DSV16BX motion and bone-conduction sensor, now available at Mouser, integrates an audio accelerometer, Qvar sensor, and UI sensor in a compact package. The device's superior performance and limited form factor make it an ideal choice for small devices, including headsets and earbuds. The LSM6DSV16BX sensor includes a triple core for processing acceleration, angular rate, and Qvar sensing data on separate channels. The "always-on" sensor features low power consumption of just 0.95 mA in combination with high-performance mode, ensuring uninterrupted performance for both the accelerometer and gyroscope. The LSM6DSV16BX device also includes a machine learning core with exportable features and filters, allowing the device to be used in AI applications.

The LSM6DSV16BX motion and bone-conduction sensor from STMicroelectronics is supported by the STEVAL-MKI234KA evaluation kit, which in conjunction with the STEVAL-MKI109V3 motherboard, provides a demonstration platform for the device. The evaluation kit supports a downloadable graphical user interface and dedicated software routines for customized applications.

To learn more about the LSM6DSV16BX motion and bone-conduction sensor from STMicroelectronics, visit https://www.mouser.com/new/stmicroelectronics/stm-lsm6dsv16bx-accelerometer-gyroscope/.

 

Hakkında STMicroelectronics

2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.