Mouser Adds Latest Wi-Fi, Cellular and GNSS Antennas from Taoglas for IoT, Smart Home, and Navigation Applications
July 23, 2025 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is stocking the newest antennas from Taoglas, a global leader in RF and wireless connectivity solutions.
The Taoglas PC60 and PC66 antennas, available from Mouser, offer a 617MHz to 6000MHz frequency range and support a wide range of 5G, 4G, and LTE cellular bands. At just 90 × 15 mm2, these antennas are the perfect solution when size constraints limit the use of a larger antenna. The flexible PC60 and PC66 antennas include a peel-and-stick adhesive backing for simple installation. Small through-holes allow for an alternative mounting option where adhesive might not be appropriate. These antennas are suitable for compact IoT devices, remote monitoring and security cameras, point-of-sale terminals, and more.
The Olympian III antennas are high-performance combination permanent mount antennas in a rugged, IP67-rated enclosure. The Olympian III antennas are offered in three variants. The MA182 offers 4G-5G MIMO connectivity, covers all worldwide LTE bands, and offers 3G/2G fallback when needed. The MA181 adds a GPS/GLONASS/Galileo antenna for positioning and location applications. The MA183 includes a wideband Wi-Fi® antenna covering the Wi-Fi 6/7 frequencies, along with the legacy 2.4/5.8GHz Wi-Fi and Bluetooth frequencies. The Olympian III series is ideal for smart metering, digital signage, transportation, and telematics.
The Taoglas HP2356.A Inception series is a low-profile GNSS patch antenna designed for optimum positional accuracy and positioning. The HP2356.A Inception utilizes an innovative ceramic patch within a patch antenna design with optimized gain for GPS L1/L2, Galileo, GLONASS and BeiDou bands and has a compact 35 × 35 mm2 footprint. At only 6 mm in height, the Inception antenna can be used in applications where typical stacked patch designs are too tall for the device.
The AA.185 Magma magnetic/adhesive mount antenna offers GPS, GLONASS, Galileo, and BeiDou L1/E1/B1 coverage in a robust ASA IP67-rated enclosure, allowing it to be used internally or externally in challenging environments. At only 35.7 mm square and 15 mm in height, the Magma antenna is well-suited for installations where durability and small size are crucial. Both the Inception and Magma antennas are ideal for applications such as telematics, fleet management, asset trackers, precision agriculture, and autonomous vehicles and robotics.
To learn more about Taoglas antennas available from Mouser, visit https://www.mouser.com/manufacturer/taoglas/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
2026 - Taoglas is a leading provider of antennas, advanced IoT components, and custom design services that help customers navigate complex RF and wireless systems and bring connectivity solutions to market on time, the first time. Since its foundation in 2004, the global company remains committed to continuous innovation, proactive customer service, and trusted quality that delivers long-term peace of mind to customers and colleagues, creating time and space to work together to advance global connectivity.