Now at Mouser: u-blox NORA-W30 Multiprotocol Modules for Efficient Wireless Connectivity

Hemen Yayınlanması İçin

Bizimle İletişime Geçin


July 16, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the NORA-W30 multiprotocol modules from u-blox. The NORA-W30 modules support Wi-Fi and Bluetooth® connectivity in a single, compact unit. The NORA-W30 devices support a range of applications, including industrial automation, metering and utilities, healthcare, smart homes, and electrical vehicle charging.

The u-blox NORA-W30 multiprotocol modules, now available at Mouser, support Wi-Fi 4 on both 2.4 and 5 GHz bands. The modules can function as a Wi-Fi station connecting to a remote access point or act as an access point. The NORA-W30 modules are Bluetooth Low Energy-qualified and can assume central or peripheral roles or both simultaneously. The modules feature a dual-core microcontroller with an Arm® Cortex®-M33 compatible processor for main applications and an Arm Cortex-M23 compatible processor for low-power operations. The NORA-W30 modules offer a robust collection of hardware security features, including secure boot, encrypted flash, debug port protection, a crypto acceleration engine, and a trusted execution environment with Arm TrustZone®. Wireless communication can be secured with WPA2/WPA3 authentication, TLS 1.2/1.3 encryption, Bluetooth LE secure connection pairing, and HTTPS.

The NORA-W30 multiprotocol modules are offered in two variants. NORA-W306 comes with an internal PCB antenna, while NORA-W301 has a module pin to connect to an external antenna of choice. The internal PCB antenna provides a robust, low-profile solution with high performance and an extensive range. The NORA-W30 series is globally certified for use with the internal antenna or a range of external antennas. This reduces time, cost, and effort for customers who are integrating Wi-Fi and Bluetooth LE into their designs.

To learn more, visit https://www.mouser.com/new/u-blox/u-blox-nora-w30-multiprotocol-modules/.

 

About u-blox

2026 - u-blox is a global provider of leading positioning and wireless communication technologies for the automotive, industrial, and consumer markets. u-blox solutions let people, vehicles, and machines determine their precise position and communicate wirelessly over cellular and short-range networks.