Analog Devices Blackfin ADZS-BF706-EZMINI Audio Evaluation Board Now at Mouser

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Analog Devices Blackfin ADZS-BF706-EZMINI Audio Evaluation Board Now at Mouser

April 27, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the ADZS-BF706-EZMINI Evaluation Board from Analog Devices. The Evaluation Board aids in the development and testing of the 32-bit, 400 MHz ADSP‑BF706 Blackfin DSP that delivers 800 MMACS of processing power at less than 100 mW. This mini evaluation board contains all the communication interfaces and external connections needed for DSP audio application design, including an Arduino‑compatible interface.

The Analog Devices' Evaluation Board, available from Mouser Electronics, offers a complete, small-form-factor, low-cost starter platform for evaluation of the Blackfin DSP processor. The features on-board, high-quality audio I/O, 1,160 KBytes of on‑chip internal SRAM, 4 MBytes of quad SPI Flash and connections for EPPI0, SPORT, SPI, I2C, and general-purpose I/O (GPIOs). The USB bus-powered board also features an on-board JTAG/SWD debug port through a separate USB interface, and an ADAU1761 SigmaDSP® low power stereo audio codec. The ADZS-BF706-EZMINI board also accommodates the installation of 0.1-inch stackable headers for interfacing with Arduino‑compatible shields that are compliant with the Arduino™ Uno R3 shields interface.

When used with the Analog Devices CrossCore Embedded Studio (CCES), the Evaluation Board offers advanced application code development and real-time debug capabilities. The CCES development environment allows designers to create, compile, assemble, and link application programs written in C, C++, and assembly code. The software package also includes DSP Concepts' graphical-based Audio Weaver software tool that provides a full-featured audio module library with efficient code generation and profiling.

The Mini Evaluation Board and ADSP-BF706 Blackfin processor targets power-sensitive embedded applications from portable audio to sound processing and effects.

To learn more, about the ADZS-BF706-EZMINI Evaluation Board, visit:
http://www.mouser.com/new/Analog-Devices/analog-adsp-bf706-board/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Analog Devices Inc.

2026 - Analog Devices, Inc. is a global semiconductor leader that bridges the physical and digital worlds to enable breakthroughs at the Intelligent Edge. ADI combines analog, digital, and software technologies into solutions that help drive advancements in digitized factories, mobility, and digital healthcare, combat climate change, and reliably connect humans and the world. With revenue of more than $12 billion in FY22 and approximately 25,000 people globally working alongside 125,000 global customers, ADI ensures today’s innovators stay Ahead of What’s Possible.