Mouser Electronics Now Shipping IDT’s ZWIR4532 Low-Power 6LoWPAN Module
December 27, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the ZWIR4532 6LoWPAN communications module from IDT®. Incorporating an Arm® microcontroller, a sub-GHz radio transceiver, and optional license-free IDT firmware download, the module enables sensors and other small devices to operate autonomously or connect to local or global IPv6 networks.
The IDT ZWIR4532 communication module, available from Mouser Electronics, is a secure, programmable connectivity module based on an ultra-low-power 32-bit Arm Cortex®-M0+ microcontroller with 128 Kbytes of flash and 4 Kbytes of RAM. The FCC-certified module provides critical and secure 6LoWPAN wireless connectivity to link devices to the Internet of Things (IoT). The module can create self-healing, ad-hoc mesh networks for covering large areas and long ranges, and features secure connectivity based on the IPSec protocol suite.
The ZWIR4532 module is available with optional IDT SensorShare™ firmware — a 6LoWPAN open standard stack that communicates natively with IPv6 over IEEE 802.15.4 radio links. The firmware has no associated license fees or royalties, allowing engineers to focus on their applications without the burden of building IoT solutions from the ground up.
The ZWIR4532 communication module has a supply voltage of 1.8 V to 3.3 V, with a network stack designed to consume minimal power in active mode. The module provides an ultra-low-power suspend mode, which turns off the transceiver and most microcontroller peripherals to lower total power consumption to less than 1 µA for battery-powered devices. The IDT ZWIR4532 6LoWPAN communications module is ideal for industrial and home automation, health monitoring, and telemetry applications.
To learn more, visit www.mouser.com/idt-zwir4532-module.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
2026 - Renesas / IDT develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, timing, wireless power transfer, serial switching, interfaces, automotive ASICs, battery management ICs, sensor signal conditioner ICs and environmental sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments.