Laird Connectivity’s BL653 Series Modules, Now at Mouser, Support Long-Range BLE Applications in Harsh Environments

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Laird Connectivity’s BL653 Series Modules, Now at Mouser, Support Long-Range BLE Applications in Har

June 30, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the BL653 Series of modules from Laird Connectivity. Featuring a comprehensive range of configurable interfaces as well as an extended industrial temperature rating, the BL653 provides reliable Bluetooth® 5.1 connectivity and support for NFC and 802.15.4 communication (Thread and Zigbee) for a range of Internet of Things (IoT) applications in industrial settings and other harsh environments.

The Laird Connectivity BL653 Series modules, available from Mouser Electronics, are small modules that deliver Bluetooth 5.1 connectivity, longer range, multi-wireless capabilities, and an extended temperature range up to 105 degrees Celsius. Powered by the compact Nordic nRF52833 system-on-chip (SoC), BL653 modules capitalize on the SoC's 64 MHz Arm® Cortex®-M4 with FPU, high output power of up to +8 dBm, and excellent sensitivity of -95 dBm sensitivity in 1 Mbps.

The modules offer Bluetooth 5.1 features such as direction finding with angle of arrival (AoA) and angle of departure (AoD), as well as long-range (Coded PHY) and 2M PHY support for data rates of 2 Mbits per second (Mbps), 1 Mbps, and 125 Kbps. The 15 mm × 10 mm × 2.2 mm modules also support flexibility in application design, enabling developers to choose between Laird Connectivity's smartBASIC, simple AT command set, Nordic SDK, or Zephyr RTOS. The module family includes integrated PCB trace antenna options for overall design simplicity or Trace Pad variants for connecting a range of pre-certified internal and external antenna options.

The BL653 includes modular FCC, IC, CE, RCM, MIC, and Bluetooth SIG approvals, which extend to an OEM's design with no new testing for the fastest route to production. Design engineers can take advantage of the fully featured BL653 development kit, available with either an internal antenna or a range of pre-certified external FlexPIFA antenna, which provides the necessary tools to begin Bluetooth Low Energy development.

To learn more about Laird Connectivity's BL653 Series, visit https://www.mouser.com/new/laird-connectivity/laird-bl653-module/.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Hakkında Laird

2026 - Laird is a global leader in solving electromagnetic interference challenges and providing state-of-the-art wireless communication and smart system solutions. The company’s products are engineered with unparalleled innovation and precision and are supplied to major companies around the world, equipping them with the technology needed to improve their business and contribute to the progress of the modern world. Laird meets the needs of a variety of industries and applications, delivering transformational solutions for a constantly changing digital society.
CONNECT - Stay wired at all times with our highly reliable power products and industrial communications systems.
PROTECT - Keep heat and electromagnetic interference at bay with high quality performance materials.
DESIGN - Design custom parts and solutions or build your entire concept from prototype to production