Mouser Electronics Now Shipping the Maxim MAXREFDES89# DC Motor Driver mbed Shield

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Mouser Electronics Now Shipping the Maxim MAXREFDES89# DC Motor Driver mbed Shield

February 2, 2016 - Mouser Electronics, Inc. is now stocking the MAXREFDES89# full-bridge DC motor driver ARM® mbed® shield from Maxim Integrated. The MAXREFDES89# provides developers with a rapid prototyping and development platform for driving up to four brushed DC motors. The board is an mbed-compatible, Arduino-form-factor shield for the rapid development of brushed DC motor applications.

The Maxim MAXREFDES89# shield, available from Mouser Electronics, contains four MAX14871 full-bridge DC motor drivers, one MAX17501 DC-DC converter, four MAX4704 low-voltage 4:1 analog multiplexers, two MAX5387 low-voltage digital potentiometers, and one MAX7300 I/O expander. Each MAX14871 driver provides the necessary functions to drive a brushed DC motor, while the additional parts allow for complete testing and operation in a variety of configurations.

The MAXREFDES89# features a supply voltage range of 7V to 36VDC, depending on the motors used, which can have a continuous current of up to 2A per driver. Developers can use an available mbed shield library, which abstracts the details of interfacing with the supporting hardware of the reference design, to simplify development. The simplicity of brushed motors and the robustness of the MAXREFDES89# shield combine for an ideal solution for prototyping robotics, gaming machines, and industrial automation projects.

To learn more, visit http://www.mouser.com/new/maxim-integrated/maxim-maxrefdes89/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Maxim Integrated

2026 - Maxim Integrated, an engineer's engineering company, exists to solve the designer's toughest problems in order to empower design Innovation. The company's broad portfolio of high-performance semiconductors, combined with world-class tools and support, delivers essential analog solutions including efficient power, precision measurement, reliable connectivity and robust protection along with intelligent processing. Designers in application areas such as automotive, communications, consumer, data center, healthcare, industrial and IoT trust Maxim to help them quickly develop smaller, smarter and more secure designs. Learn more at https://www.maximintegrated.com.