NXP’s MRFX1K80H Transistor, Now at Mouser, Helps Speed RF Power Design with 65V LDMOS Technology

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


NXP’s MRFX1K80H Transistor, Now at Mouser, Helps Speed RF Power Design with 65V LDMOS Technology

September 21, 2017 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MRFX1K80H LDMOS transistor from NXP® Semiconductors. The MRFX1K80H is part of the MRFX series of radio frequency (RF) MOSFET transistors that incorporate a new laterally diffused metal oxide semiconductor (LDMOS) technology. The LDMOS technology found in the MRFX1K80H helps increase the output power in wideband applications while maintaining appropriate output impedance.

The NXP MRFX1K80H LDMOS transistor, available from Mouser Electronics, is designed to deliver 1800 W of a continuous wave at 65 V for RF applications from 1.8 to 470 MHz with the ability to handle a voltage standing wave ratio (VSWR) of 65-to-1 at all phase angles. The device offers impedance matching to 50 Ohms, helping to reduce the overall development time. Designed for an extended power range from 30V to 65V, the MRFX1K80H features a high breakdown voltage that provides enhanced reliability and higher efficiency. The high voltage lowers the current in the system, limiting the stresses on DC power supplies thereby reducing magnetic radiation. The higher output power also helps decrease the number of transistors to combine and simplify the power amplifier complexity and reduce the overall size.

The MRFX1K80H is suitable for linear applications with appropriate biasing and offers integrated electrostatic discharge (ESD) protection for improved Class C operation. Target applications for the MRFX1K80H include industrial, scientific, and medical (ISM) applications as well as broadcast, aerospace, and mobile radio equipment.

To learn more about NXP's MRFX1K80H LDMOS transistor, visit http://www.mouser.com/new/nxp-semiconductors/nxp-mrfx1k80/.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Hakkında NXP Semiconductors

2026 - NXP Semiconductors enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security and privacy and smart connected solutions markets.