Now at Mouser: TE Connectivity’s HTU31 High-Accuracy Humidity & Temperature Sensors for Harsh Environments
September 30, 2020 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now offering the new HTU31 relative humidity sensors from TE Connectivity (TE), a world leader in connectivity and sensors. One of the smallest and most accurate humidity sensors on the market, the compact, high-accuracy sensors deliver reliable performance in harsh environments, including in industrial, automotive, and medical applications.
TE's HTU31 devices — now shipping from Mouser in a digital version, with an analog version coming soon — are surface mount relative humidity sensors with a temperature output. The sensors offer fast response times, precision measurement, and low hysteresis, even when exposed to extreme temperature and humidity environments. The sensors have an operating temperature range of minus 40 degrees to 125 degrees Celsius with a typical accuracy of ±0.2 degrees. Measuring relative humidity from 0 to 100 percent, the sensors offer resolution to 0.01 and an accuracy of ±2 percent.
The HTU31 sensors feature an operating voltage range of 3.3 V to 5.5 V, and maintain an active current consumption of just 450 µA, with sleep modes down to 0.05 µA. The sensors are qualified according to AEC Q100 Grade 1 standards and are housed in a compact, 6-pin DFN package measuring 2.5 mm × 2.5 mm × 0.9 mm. In addition to harsh environment performance, the sensors are also suitable for applications such as HVAC, home appliances, respiratory devices, and environmental monitoring solutions.
To learn more about the HTU31 Relative Humidity Sensors from TE Connectivity, visit https://www.mouser.com/new/measurement-specialties/te-htu31-relative-humidity-sensors/.
2026 - TE Connectivity plc is a global industrial technology leader creating a safer, sustainable, productive, and connected future. As a trusted innovation partner, its broad range of connectivity and sensor solutions enables the distribution of power, signal, and data to advance next-generation transportation, energy networks, automated factories, data centers enabling artificial intelligence, and more.
TE's more than 90,000 employees, including 10,000 engineers, work alongside customers in approximately 130 countries. In a world that is racing ahead, TE ensures that EVERY CONNECTION COUNTS.