Mouser Electronics Stocks Xilinx Zynq UltraScale+ Dual- and Quad-Core Multiprocessor SoCs

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Mouser Electronics Stocks Xilinx Zynq UltraScale+ Dual- and Quad-Core Multiprocessor SoCs

October 1, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking Zynq® UltraScale+ multiprocessor system-on-chips (MPSoCs) from Xilinx.

Xilinx Zynq UltraScale+ devices, available from Mouser Electronics, combine a high-performance Arm®-based multicore, multiprocessing system with ASIC-class programmable logic. The devices deliver maximum scalability, and can offload critical applications, such as graphics and video pipelining, to dedicated processing blocks. The MPSoCs also include a full complement of integrated peripherals and connectivity cores suitable for next-generation applications such as 5G wireless, automotive ADAS, and industrial Internet of Things (IoT).

The Zynq UltraScale+ family of MPSoCs comprises three distinct variants (CG, EG, and EV), each of which includes two or four Arm Cortex®-A53 cores and two Arm Cortex-R5 real-time processing units. The dual-core CG devices are optimal for industrial motor control and sensor fusion. Both the EG series and EV series devices feature four Cortex-A53 cores, as well as an Arm Mali-400 graphics processing unit. The EV series also includes a video codec unit that supports H.265 High Efficiency Video Coding (HEVC) and H.264 Advanced Video Coding (AVC) standards, making them ideal for multimedia, ADAS, and surveillance applications.

To learn more about the Xilinx Zynq UltraScale+ MPSoCs, visit www.mouser.com/xilinx-zynq-ultrascale-mpsocs.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Hakkında AMD / Xilinx

2026 - AMD / Xilinx develops highly flexible and adaptive processing platforms that enable rapid innovation across a variety of technologies, from the endpoint to the edge to the cloud. Specializing in programmable logic devices, Xilinx is the semiconductor company that invented the Field Programmable Gate Array (FPGA), the hardware programmable System on Chip (SoC), and the Adaptive Compute Acceleration Platform (ACAP).