Mouser Electronics Now Stocking the STMicroelectronics IIS3DWBG1 Vibration Sensor

Yeni Ürün Basın Özeti

Bizimle İletişime Geçin


Learn more about the IIS3DWBG1 vibration sensor
Learn more about the IIS3DWBG1 vibration sensor

January 15, 2026 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the IIS3DWBG1 vibration sensor from STMicroelectronics.

The IIS3DWBG1 is a 3-axis digital vibration sensor with low noise over an ultrawide and flat frequency range. This sensor offers a selectable full-scale acceleration range of ±2 g, ±4 g, ±8 g, or ±16 g and is capable of measuring accelerations with a bandwidth of up to 6kHz. The IIS3DWBG1 vibration sensor delivers high performance with low power consumption, featuring a digital output. This sensor integrates a 3kB First-In, First-Out (FIFO) buffer to prevent data loss and reduce host processor intervention. The IIS3DWBG1 vibration sensor features an ultralow noise density of 75 µg/√Hz in 3-axis mode and 60 µg/√Hz in single-axis mode. This sensor is available in a 14-lead plastic, Land Grid Array (LGA) package.

Typical applications include industrial equipment, electric and hybrid vehicles, condition monitoring, test and measurements, and predictive maintenance.

To learn more, visit https://www.mouser.com/new/stmicroelectronics/stmicroelectronics-iis3dwbg1-vibration-sensor/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Hakkında STMicroelectronics

2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.