Nordic Semiconductor's nRF52820 Multi-protocol SoC, Now at Mouser, Combines Bluetooth 5.2 with USB 2.0
September 23, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the nRF52820 multi-protocol system-on-chip (SoC) from Nordic Semiconductor. With support for the full suite of Bluetooth® 5.2 features and other popular communications protocols, the SoC is an ideal solution for a variety of wireless Internet of Things (IoT) applications, including asset tracking, high-performance human interface device (HID) controllers, smart home products, and professional lighting.
The Nordic nRF52820 SoC, available from Mouser Electronics, is based on Nordic's nRF52 Series architecture and supports Bluetooth® 5.2, Bluetooth Low Energy, and Bluetooth mesh, as well as Direction Finding, high-throughput 2 Mbps, and Long Range features. The SoC also supports Thread, Zigbee®, and 2.4-GHz proprietary communications technologies along with Full Speed USB 2.0 connectivity in a single-chip solution.
The ultra-low-power Arm® Cortex®-M4-based SoC is drop-in compatible with Nordic's nRF52833 SoC, offering a range of analog and digital interfaces such as an analog comparator, SPI, UART, TWI, QDEC, and Full Speed (12 Mbps) USB. The built-in USB, fully-featured multiprotocol radio and +8 dBm output power makes the nRF52820 SoC an ideal network processor to be paired with an application microcontroller in gateways and other smart home, commercial and industrial applications requiring advanced wireless connectivity.
Mouser also stocks the Nordic nRF52833 Development Kit, based an onboard nRF52833 SoC that emulates the features of the nRF52820 SoC. The kit offers four user-programmable buttons and LEDs, is hardware compatible with the Arduino Uno R3-based shields, and features connector pins for all inputs and outputs (I/O) and interfaces, including a dedicated connector for the included external NFC antenna.
To learn more, visit https://www.mouser.com/new/nordic-semiconductor/nordic-nrf52820/.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 1,100 manufacturer brands. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit www.mouser.com.
About Nordic Semiconductor
Nordic Semiconductor provides class-leading levels of wireless performance and sophistication at a price that enables the company's ultralow power (ULP) wireless chips to be used in even the most cost-sensitive consumer products. Nordic Semiconductor's chips can be found in products such as wireless PC peripherals, gaming controllers, sports and fitness sensors, toys, advanced multi-media controllers, and digital/satellite TV (set-top box) remotes and much more.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com