Use USB Faster with the Cypress EZ USB FX3 USB 3.0 SuperSpeed Explorer Kit Available from Mouser

Hemen Yayınlanması İçin

Bizimle İletişime Geçin


Use USB Faster with the Cypress EZ USB FX3 USB 3.0 SuperSpeed Explorer Kit Available from Mouser

February 17, 2015 - Mouser Electronics, Inc. is now stocking the EZ-USB® FX3™ USB 3.0 SuperSpeed Explorer Kit from Cypress Semiconductor. This Explorer Kit includes all the hardware, software, and documentation necessary to enable developers to evaluate the Cypress EZ-USB® FX3™, an ARM‑based USB 3.0 peripheral controller. USB 3.0 offers the SuperSpeed signaling rate of 5 Gigabits per second, ten times greater than the USB 2.0 high-speed signaling rate of 480 megabits per second.

The Cypress EZ-USB FX3 SuperSpeed Explorer Kit, available from Mouser Electronics, allows developers to add USB 3.0 SuperSpeed connectivity to any design. The development board provides convenient access to all FX3 IC interfaces. Two 40-pin headers allow the FX3 to connect to external boards using the Cypress's 2nd generation General Programming Interface (GPIF‑II). These headers use long pins that can also be used as test points. The board can connect to external devices such as FPGAs, CPLDs, image sensors, or microcontrollers. The FX3 Software Development Kit (SDK) includes example code to help learn how to program and evaluate the FX3. The SuperSpeed Explorer kit easily interfaces to Altera FPGAs as well as image sensor peripheral boards.

The USB 3.0 SuperSpeed Explorer Kit development board provides two USB connectors. The USB 3.0 Type‑B connector brings out the FX3 USB signals. This connector can accept either a USB 3.0 or USB 2.0 connector. A USB 2.0 Micro-B receptacle interfaces to an onboard Cypress CY7C65215 USB‑Serial Dual Channel UART/I2C/SPI Bridge, which is configured as the board's integrated debugger operating at the USB 2.0 Full-Speed rate. This chip provides a bridge between the FX3 debug interface and a PC's USB port, enabling serial terminal message debugging as well as JTAG debugging.

The kit also includes the Cypress EZ USB Suite, ARM GCC toolchain, FX3 firmware library, and example projects. Also included is the Cypress USB Suite and sample Microsoft Visual Studio applications. A USB 3.0 cable is included.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Cypress Semiconductor

2026 - Cypress is the leader in advanced embedded system solutions for the world's most innovative automotive, industrial, smart home appliances, consumer electronics and medical products. Cypress' microcontrollers, analog ICs, wireless and USB-based connectivity solutions and reliable, high-performance memories help engineers design differentiated products and get them to market first. Cypress is committed to providing customers with the best support and development resources on the planet enabling them to disrupt markets by creating new product categories in record time.