Mouser Now Stocking Cypress PSoC 4XX8_BLE Controllers for Sensor-Based IoT Applications
October 13, 2016 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the PSoC® 4XX8_BLE embedded system controllers from Cypress Semiconductor. Containing the same core features as Cypress' popular PSoC 4 family of embedded system controllers, these highly integrated, single-chip Bluetooth® low energy (BLE) solutions also add a 2.4 GHz radio core that makes the devices compliant with Bluetooth Smart Specification 4.2. The PSoC 4XX8_BLE programmable system-on-a-chip (PSoC) devices integrate BLE with a 32-bit ARM® Cortex®-M0 core and deliver a highly scalable and configurable low-cost, single-chip alternative to microcontrollers and external ICs typically required for similar functionality.
The Cypress PSoC 4XX8_BLE embedded system controllers, available from Mouser Electronics, incorporate programmable and reconfigurable analog and digital blocks with flexible automatic routing. The microcontroller subsystem features a 48-MHz ARM Cortex-M0 CPU, up to 256 kBytes of flash, up to 32 kBytes of SRAM, CapSense® capacitive-sensing technology, and multiple low-power modes — including active, sleep, deep-sleep, hibernate, and stop — which are especially useful for Internet of Things (IoT) applications. All PSoC 4XX8_BLE devices include a royalty-free BLE protocol stack compatible with Bluetooth 4.2, and are fully upward compatible with other members of Cypress' PSoC 4 platform.
The PSoC4XX8_BLE family of devices is supported by the CY8CKIT-042-BLE-A Bluetooth® Low Energy Pioneer Kit and the PSoC Creator™ integrated design environment, which enables complete system design in a single tool. The BLE Pioneer Kit offers footprint-compatibility with Arduino shields as well as 6-pin Digilent Pmod™ daughter cards. In addition, the kit features a CapSense slider and an onboard programmer/debugger (KitProg) with USB-UART/I2C bridge functionality. The Cypress PSoC 4XX8_BLE embedded system controllers deliver unprecedented ease-of-use and integration to simplify the design of low-power, sensor-based systems for the IoT. Target applications include home automation, healthcare equipment, sports and fitness monitors, and wearable devices.
To learn more about the Cypress PSoC 4XX8_BLE embedded system controllers, visit http://www.mouser.com/new/Cypress-Semiconductor/cypress-psoc4xx8-ble-controllers/. For more information on the CY8CKIT-042-BLE-A Bluetooth Low Energy Pioneer Kit, go to http://www.mouser.com/new/Cypress-Semiconductor/cypress-ble-pioneer-kit/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
2026 - Cypress is the leader in advanced embedded system solutions for the world's most innovative automotive, industrial, smart home appliances, consumer electronics and medical products. Cypress' microcontrollers, analog ICs, wireless and USB-based connectivity solutions and reliable, high-performance memories help engineers design differentiated products and get them to market first. Cypress is committed to providing customers with the best support and development resources on the planet enabling them to disrupt markets by creating new product categories in record time.