Mouser Electronics Now Stocking Texas Instruments’ OPA855 8-GHz Operational Amplifier

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Mouser Electronics Now Stocking Texas Instruments’ OPA855 8-GHz Operational Amplifier

July 3, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the OPA855 decompensated amplifier from Texas Instruments (TI). Designed as a wideband, low-noise, bipolar-input operational amplifier, the OPA855 excels in high bandwidth transimpedance and voltage amplifier applications. The 8-GHz gain-bandwidth product (GBWP) of the OPA855 enables high-gain configurations while maintaining wide closed-loop bandwidth. Additionally, the low input-voltage noise of 0.98 nV/√Hz minimizes noise contribution from the amplifier, and the high slew rate of 2750 V/µs enables wide output voltage swings.

For transimpedance amplifier (TIA) applications TI's OPA855, available from Mouser Electronics, features a low input capacitance of only 0.8 pF, which minimizes the total circuit input capacitance and enables higher-speed designs. The device also uses a unique package pinout that simplifies the layout of the feedback network while simultaneously isolating pin-to-pin capacitance between the input and feedback connections. This pinout design reduces the total parasitic capacitance around the amplifier's feedback network, allowing for high-gain TIA designs to achieve wide bandwidth.

TIA applications for the OPA855 include in optical time-of-flight (ToF) systems with a time-to-digital converter, such as TI's TDC7201. Alternatively, the OPA855 can also be used to drive a high-speed analog-to-digital converter (ADC) in high-resolution LIDAR systems with a differential output amplifier, such as TI's THS4541 or LMH5401.

The OPA855 is the latest addition to TI's family of ultra-wide bandwidth operational amplifiers, which also includes the FET-input OPA858 and OPA859 devices. This family of amplifiers is ideal for wideband transimpedance circuits as well as high-speed data acquisition systems, low-noise front ends, and more. The device is supported by the dedicated OPA855DSGEVM op amp evaluation module and the general-purpose DEM-OPA-WSON8-EVM unpopulated evaluation board./p>

To learn more, visit www.mouser.com/ti-opa855-amplifiers.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Hakkında Texas Instruments

2026 - Texas Instruments Incorporated is a global semiconductor company that designs, manufactures, and sells analog and embedded processing chips for markets such as industrial, automotive, personal electronics, enterprise systems, and communications equipment. At its core, Texas Instruments has a passion to create a better world by making electronics more affordable through semiconductors. This passion is alive today as each generation of innovation builds upon the last to make the company's technology more reliable, more affordable, and lower power, making it possible for semiconductors to go into electronics everywhere.