Dialog DA16600 Wi-Fi and BLE Modules Now at Mouser

Yeni Ürün Basın Özeti

Bizimle İletişime Geçin


June 7, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the DA16600 Wi-Fi and Bluetooth® Low Energy modules from Dialog Semiconductor.

Dialog DA16600 modules provide a convenient way to add both low-power Wi-Fi and low-power Bluetooth Low Energy functionality to applications. The DA16600 modules are based on the VirtualZero™ DA16200 Wi-Fi system-on-chip (SoC) and the SmartBond TINY™ DA14531 Bluetooth Low Energy SoC. Together they deliver long battery life and low power consumption in a convenient form factor. As a single integrated system, functions such as Wi-Fi/Bluetooth Low Energy coexistence and provisioning Wi-Fi through the Bluetooth Low Energy connection come standard.

The DA16600 modules are complete with all required components and are certified by the FC, IC, CE, and other regulatory bodies. 

For more information, visit https://www.mouser.com/new/dialog-semiconductor/dialog-da16600-wifi-ble-module/.