Go Micro with New Bosch BMA530 and BMA580 MEMS Accelerometers from Mouser

World's Smallest Accelerometers Offer Big Performance
Yeni Ürün Duyurusu

Bizimle İletişime Geçin


Bosch BMA530 and BMA580 accelerometers

July 3, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the new BMA530 and BMA580 accelerometers from Bosch. The BMA530 and BMA580 are some of the world's smallest acceleration sensors for space-constrained applications like wearables and hearables.

The Bosch BMA530 and BMA580 accelerometers, available from Mouser, offer big performance in one of the industry's smallest packages for design engineers requiring easy implementation without detailed application knowledge. Built-in features enable the BMA530 to track motion activities with a step counter that is especially suitable for wearables. At the same time, the BMA580 targets hearables with voice activity detection that features bone conduction. Typically, microphones consume a lot of power in hearables because they need to be "always-on" to listen for voice activity, but bone conduction detects the vibration of the user's voice to wake the device from sleep for increased power savings in a miniature sensor size.

Compared to Bosch's previous generation accelerometers, the BMA530 and BMA580 have a 76 % smaller footprint (down from 0.95 mm to 0.55 mm.) in an innovative Wafer Level Chip Scale Package (WLCSP), making them easy to place on a PCB and integrate into portable products, while offering a flexible set of connectivity options, including an I3C® interface.

The BMA530 and BMA580 accelerometers are supported by the BMA530 and BMA580 shuttle boards, available for order from Mouser. The shuttle boards, when used in conjunction with the Bosch Application board which is available to order, provide an example application circuit, allowing rapid prototyping when incorporated into existing designs.

To learn more about the BMA530, visit https://www.mouser.com/new/bosch/bosch-bma530-accelerometers/.

To learn more about the BMA580, visit https://www.mouser.com/new/bosch/bosch-bma580-accelerometers/.

 

Hakkında Bosch

2026 - The Bosch Group, a leading global supplier of technology and services, is designed to improve quality of life worldwide with products and services that are innovative and spark enthusiasm.