STMicroelectronics’ LIS2DUX12 and LIS2DUXS12 Smart Accelerometers, Now Available at Mouser, Increase Efficiency for Wearables
May 3, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the LIS2DUX12 and LIS2DUXS12 AI-enhanced smart accelerometers from STMicroelectronics. Leveraging STMicroelectronics' third-generation MEMS technology, the accelerometers accurately detect events and gestures with high accuracy and low power consumption. The new smart accelerometers support a range of "always-aware" applications, including wearable devices, game controllers, portable healthcare devices, asset trackers, and wireless sensor nodes. These AI-enhanced devices also include a machine learning core with adaptive self-configuration, offloading host processing and enabling faster system responses.
The STMicroelectronics LIS2DUX12 AI-enhanced smart accelerometer, now available at Mouser, is a smart, digital, 3-axis linear accelerometer. The LIS2DUX12 MEMS and ASIC combine low current consumption with always-on anti-aliasing filtering and a finite state machine. The highly versatile accelerometer includes four performance modes, including a high-performance mode with an anti-aliasing filter of 10.8 µA, a low-power mode with an anti-aliasing filter of 6.2 µA, an ultra-low power mode of 2.7 µA, and a power-down mode at just 0.01 µA.
The LIS2DUXS12 AI-enhanced smart accelerometer includes STMicroelectronics' unique Qvar® sensing channel and analog hub, which senses changes in the ambient electrostatic environment to enable presence and proximity detection. The Qvar sensing channel allows developers to add value to applications, including liquid detection, biometric sensing, and user-interface control.
To learn more about the LIS2DUX12 AI-enhanced smart accelerometer from STMicroelectronics, visit https://www.mouser.com/new/stmicroelectronics/stm-lis2dux12-accelerometer/.
To learn more about the LIS2DUXS12 AI-enhanced smart accelerometer, visit https://www.mouser.com/new/stmicroelectronics/stm-lis2duxs12-accelerometer/.
2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.