Mouser Electronics Stocks Wide Selection of Over 20,000 Products from TDK Corporation
December 7, 2022 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is an authorized global distributor of solutions from TDK Corporation. Mouser offers customers over 20,000 parts in stock from TDK and its companies EPCOS, InvenSense, Micronas, Tronics, and TDK-Lambda.
Mouser offers a wide range of products from TDK, including semiconductors, optoelectronics, sensors, and passive components. The following are just a few of the TDK products available from Mouser:
μPOL™ DC-DC power modules are compact and highly integrated point-of-load converters. The high-current-density power modules provide the high performance, fast load transient response, and high-accuracy voltage regulation needed to power CPUs, MCUs, ASICs, FPGAs, DSPs, and other advanced digital logic devices. µPOL converters feature a chip-embedded power IC in a thermally enhanced semiconductor-embedded-in-substrate package.
EPCOS CLT32 automotive-grade power inductors are suitable for safety-critical automotive applications in advanced driver-assistance systems (ADAS). These AEC-Q200-certified components feature a small footprint of 3.2 mm × 2.5 mm and an insertion height of 2.5 mm.
The WCT wireless charging coil features pattern coil technology that reduces thickness to cover a larger charging area in a single cell. This design, combined with TDK’s proprietary magnetic material, reduces the coil thickness to 0.76 mm.
In addition to offering a broad selection of TDK products, Mouser has received many accolades from the valued manufacturer partner, including the Global Best Performance Award for Fiscal Year 2022, North America Distributor of the Year for Calendar Year 2021, and European Distribution Award in High-Service Distribution for 2021. Mouser also received the European Distribution Award in High-Service Distribution for 2020, 2018, and 2017, as well as the Sales Achievement Award for Highest Growth Distributor for Fiscal Year 2019 and America’s Highest Percentage Sales Growth for Fiscal Year 2017.
To learn more about TDK and its product line available from Mouser, visit https://www.mouser.com/manufacturer/tdk-corp/.
2026 - TDK Corporation is a world leader in electronic solutions for smart society and is based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately "Attracting Tomorrow." It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and North and South America.