Xilinx’s Kria KR260 Robotics Starter Kit, Now at Mouser, Accelerates Workflows for Roboticists

Yeni Ürün Duyurusu

Bizimle İletişime Geçin


March 16, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is now stocking the Kria KR260 Robotics Starter Kit from Xilinx. Offering high-performance industrial vision and real-time networking interfaces, this Xilinx starter kit allows roboticists to simplify their workflows when using the Kria K26 system-on-module (SOM). The Kria KR260 Starter Kit supports a range of robotics, machine vision and industrial communication and control applications.

The Xilinx Kria KR260 Robotics Starter Kit, available at Mouser, includes a pre-installed Kria K26 SOM using two 240-pin connectors and I/Os for sensor and network connectivity. The starter kit offers exceptional industrial vision with an SLVS-EC Rx, DisplayPort 1.2a, and four USB 3.0 ports for camera interfaces. The kit’s robust collection of real-time networking interfaces includes four RJ45 Ethernet ports and one SFP+ optics interface for 10GE vision. Featuring native ROS 2 and Ubuntu support along the Kria Robotics Stack (KRS), the Kria KR260 Starter Kit supports ease of development for roboticists and embedded developers alike.

The Kria KR260 Robotics Starter Kit from Xilinx can be easily adapted and scaled using Pmod and Raspberry Pi headers. With a broad Pmod ecosystem, the kit can extend to any sensor or interface.

To learn more about the Xilinx Kria KR260 Robotics Starter Kit visit https://www.mouser.com/new/xilinx/xilinx-kria-kr260-kit/.

 

Hakkında AMD / Xilinx

2026 - AMD / Xilinx develops highly flexible and adaptive processing platforms that enable rapid innovation across a variety of technologies, from the endpoint to the edge to the cloud. Specializing in programmable logic devices, Xilinx is the semiconductor company that invented the Field Programmable Gate Array (FPGA), the hardware programmable System on Chip (SoC), and the Adaptive Compute Acceleration Platform (ACAP).